Export - CSV (All fields)
Export - CSV (Current fields)
EXT_EP-13604
MSPM33 MTB Trace in Secure Mode not supportedEXT_EP-13605
Segger J-Link supportEXT_EP-13544
F29 Disassembly view binary output is incorrect for 48-bit+ packetsEXT_EP-12243
fsclean.bat does not seem to remove targetDB cache files.EXT_EP-13483
Driver install script fails on Ubuntu 26.04EXT_EP-13229
Editor: "Go to Definition" feature can be inconsistent for linked source filesEXT_EP-13475
Hardware breakpoints are only available on the first device of multiple daisy chained devicesEXT_EP-12257
Need ability to specify where to save Target Configuration file (ccxml)EXT_EP-13532
CIO output to console is inconsistent, and sometimes GUI CIO output is not able to be established at all with a coreEXT_EP-12966
Option to export all messages in the Problems view to a log fileEXT_EP-13611
Unable to explicitly build executable project if it is shared between multiple system projectsEXT_EP-13609
Using the tiarmclang or c29clang option --version causes the build to succeed no matter whatEXT_EP-13608
Auto Indent (Format) Behavior Degraded Compared to Legacy VersionEXT_EP-13607
Launching sometimes prompts for connection selection even when connected to one boardEXT_EP-13606
Loss of focus/context during project build from AI chat window when project build is initiated by AIEXT_EP-13566
Register view still tries to read unreadable registersEXT_EP-13471
clangd: Unable to go to definition for unint16_t in C2000Ware examplesEXT_EP-13293
"Go to Definition/Declaration" fails with "No references found for <function>" for some functionsEXT_EP-13460
Target Configuration: Filter out all F29x devices for XDS100 based connection typesEXT_EP-13465
Target Configuration: Filter out all C2000 based devices for J-Link based connection typesEXT_EP-13486
Launch config properties not auto-populated when no launch config existsEXT_EP-13541
File links generated by Claude Code's AI agent in CCS opens in an external browser with an errorEXT_EP-13533
Issue in CCS 20.5 autogenerated generated makefile for multi project in F28P65EXT_EP-13504
When setting a breakpoint via a MCP call the agent should be informed where it was setEXT_EP-12145
Allow ability to select which debug probe support to installEXT_EP-13567
CCS Project dependency settings missing after switching the compiler from TI to GCCEXT_EP-13553
Do not use "-r" gmake option when using a custom build-commandEXT_EP-13564
Unable to import old CCSv4 projectsEXT_EP-13393
SysConfig file list exposed via MCP server does not match open SysConfig filesEXT_EP-13507
Launching CCS Theia installer with '--disable-components' flag fails to include component PF_WCONNEXT_EP-13550
.codex folder appears in new workspaceEXT_EP-13551
CCS AI cannot read non-core registers available in the Registers view.EXT_EP-13526
Compiler includes missing after importEXT_EP-13540
"Reconnecting to TI Cloud Agent" error occurs when trying to connect to a core on the AM62D AUDIO EVMEXT_EP-13348
Global breakpoints are not supported on F29 devicesEXT_EP-12168
Energy Trace Theia: Cannot run EnergyTrace measurements when debug session is not runningEXT_EP-13392
SysConfig MCP session can get out of sync with file on diskEXT_EP-13340
CCS Server does not initialize when CCS is installed in a folder with a unicode characterEXT_EP-13534
Show progress when archiving logsEXT_EP-13527
Request for a WHCP-signed Spectrum Digital XDS560v2 USB driverEXT_EP-13505
Prompting to reload on build causes issues when using AIEXT_EP-13466
F29: On Run/Halt don't clear the Sync Halt, Sync Run and other XRIG enable bitsEXT_EP-13468
Opening second CCS instance when Claude is enabled causes hang on startupEXT_EP-13525
Running MTB trace on MSPM0H3216 LaunchPad causes TI Cloud Agent errorEXT_EP-13524
Recurrent Git (built-in) extension error "Right-hand side of 'instanceof' is not an object"EXT_EP-13523
EnergyTrace fails to capture data on MSPM0 devices for certain variants of XDS110EXT_EP-13506
Serial Console and MCP Server do not show data even when external console doesEXT_EP-12456
Project view in target configs viewEXT_EP-10758
Unable to perform a synchronous run for grouped cores on some newer 28x devices.EXT_EP-13259
Read, reset, configure profile clock Tool API
{"errorMessages":["jqlTooComplex"],"errors":{}}
[{"id":-1,"name":"My open issues","jql":"assignee = currentUser() AND resolution = Unresolved order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":true},{"id":-2,"name":"Reported by me","jql":"reporter = currentUser() order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":true},{"id":-4,"name":"All issues","jql":"order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-5,"name":"Open issues","jql":"resolution = Unresolved order by priority DESC,updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-9,"name":"Done issues","jql":"statusCategory = Done order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-3,"name":"Viewed recently","jql":"issuekey in issueHistory() order by lastViewed DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-6,"name":"Created recently","jql":"created >= -1w order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-7,"name":"Resolved recently","jql":"resolutiondate >= -1w order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-8,"name":"Updated recently","jql":"updated >= -1w order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false}]
0.3
0