Uploaded image for project: 'Embedded Software & Tools'
  1. Embedded Software & Tools
  2. EXT_EP-11789

Source file active/inactive code highlighting is not picking up changes made to project properties for opened files

XMLWordPrintable

    • Icon: Bug Bug
    • Resolution: Unresolved
    • Icon: Medium Medium
    • Code Composer Studio Theia
    • CCSNXT-1521
    • CCS_THEIA_1.4.0
    • None
    • Close the file and reopen it.

      It appears that the clangd parser is not properly picking up predefined symbol changes made in the project properties. This is impacting proper conditional highlighting of active/inactive code in the editor.

      This only happens when the source file is already open in the editor. Closing the file and reopening it will resolve the issue.

            syncuser TI User
            syncuser TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated: