LLDB SM: Need support for clang compiled executables that use overlays

XMLWordPrintable

    • Type: Enhancement
    • Resolution: Unresolved
    • Priority: Medium

      For applications that use overlays, it was possible to debug them with CCS by leveraging GEL/DSS APIs to show and hide symbols for the appropriate sections so that the debugger would pull up the right source (and other related debug information) when debugging the overlay code. This is still applicable for non-clang compiler output that uses OFS. However this functionality is not supported with the LLDB symbol manager, making it difficult to debug overlays.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-4231 - LLDB SM: Need support for clang com...
                SYNCHRONIZED
                • Last Sync Date: