Add note regarding VMs to XDS110 firmware update message

XMLWordPrintable

    • Type: Enhancement
    • Resolution: Unresolved
    • Priority: Not Prioritized

      The automatic update of the XDS110 firmware by the debugger will fail if the user is using a VM. This is because the update process requires a reset of the XDS110 which will then cause the VM to lose connection to the XDS110 (which is not then automatically restored). This results in a update failure.

      We should add a note in the update message dialog where the user is warned against attempting the update when running from a VM.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-4400 - Add note regarding VMs to XDS110 fi...
                SYNCHRONIZED
                • Last Sync Date: