Details
-
Bug
-
Status: Accepted
-
Medium
-
Resolution: Unresolved
-
Code Composer Studio Debugger
-
CCBT-3079
-
CCS_11.1.0
-
CCS_12.5.0
-
Generic
-
Manually set the TCLK value ("Automatic with user specified limit"). 10MHz seems to work fine.
Description
Environment:
CCS 11.1.0
Blackhawk XDS560v2 USB
F28388D
Issue:
PRSC error occurs when trying to connect to the target using the default "Automatic with legacy 10.368MHz limit" TCLK setting. Interestingly, when manually setting the TCLK value to a similar value like 10MHz will work.
Workaround:
Manually set the TCLK value ("Automatic with user specified limit"). 10MHz seems to work fine.