AM64x: Cortex-M4 Core Trace: TDF file is saved incorrectly

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium
    • Debug and Trace
    • DBGTRC-6077
    • Hide
      EMU21_M01
      CCS_10.2.0
      Show
      EMU21_M01 CCS_10.2.0
    • TBD
    • XDS Device Support

      When saving the trace data as TDF the file is incorrectly created with an ITM header and cannot be re-opened by Core Trace.
      In Trace Analyzer it opens as a corrupted ITM trace. Opening the TDF only succeeds in Trace Analyzer, TVT is unable to open it and displays a blank page.

      Workaround: Saving as CSV works correctly.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-2773 - AM64x: Cortex-M4 Core Trace: TDF fi...
                SYNCHRONIZED
                • Last Sync Date: