Export - CSV (All fields)
Export - CSV (Current fields)
EXT_SITMPUSW-299
IPC notify: Null check is not handled properlyEXT_SITMPUSW-298
Spinlock: Hang in multithread test cases due to HW interrupt configEXT_SITMPUSW-297
Flash Params Not Reflected In SyscfgEXT_SITMPUSW-296
Fix issues with log in sbl_jtag_uniflashEXT_SITMPUSW-295
Flash Close Logic Requires OSPI Handle to be reset to 1S-1S-1SEXT_SITMPUSW-294
AM64: dhrystone_benchmark example for A53 core fails in debug modeEXT_SITMPUSW-293
Sciclient driver uses incorrect context for the TISCI_MSG_KEYRING_IMPORTEXT_SITMPUSW-292
Bootloader_socOpenFirewalls is called before System_init in the SBLsEXT_SITMPUSW-291
Wait for Status mechanism via Sciclient API call fails during self resetEXT_SITMPUSW-290
TX macro (AASRC_TX_DMA_TR_COUNT) used inside AASRC_udmaIsrRx (RX function)EXT_SITMPUSW-289
Uniflash script fails when trying to erase sector or size 4MBEXT_SITMPUSW-288
LPM: Unable to enter LPM in Interrupt ModeEXT_SITMPUSW-287
Spinlock: Missing NULL Pointer Validation for Base Address Parameter in Spinlock APIsEXT_SITMPUSW-286
AM275: RM boardcfg changes are not taking effectEXT_SITMPUSW-285
AASRC driver bug: AASRC_MAX_OUT_FIFO_THRESHOLD set to 16UEXT_SITMPUSW-283
WDT: Hang due to no valid argument check in APIsEXT_SITMPUSW-282
Sysconfig not generating code for GPIO TriggerEXT_SITMPUSW-281
UART: UART_open fails when NULL argument is passed as UART_Params argumentEXT_SITMPUSW-280
OSPI Indac Mode Should Check for odd bytesEXT_SITMPUSW-279
I2C close is not working properly during error conditionsEXT_SITMPUSW-277
MCASP: tx.evtCtl Used Instead of rx.evtCtl for REVTCTL ConfigurationEXT_SITMPUSW-276
MCASP: intCfgTx.intrNum Used Instead of intCfgRx.intrNum in Interrupt CheckEXT_SITMPUSW-275
Debian SDK: support for graphics user mode librariesEXT_SITMPUSW-274
MCU+SDK build is failing due to "TSN generated folder" missingEXT_SITMPUSW-273
AM64x PCIe as End Point throwing error when changing BAR apertureEXT_SITMPUSW-272
AM273x: ENET: TCP Server example needs second reset to successfully run the applicationEXT_SITMPUSW-271
Build failure with networking examples from mcu_plus_sdk inside ind_comms_sdkEXT_SITMPUSW-270
Enabling MAC2MAC/NO-PHY in networking examples gives build errorEXT_SITMPUSW-269
LPDDR: DDR PLL reset code issueEXT_SITMPUSW-268
Fix DSS timing issue for sil9022a bridge driverEXT_SITMPUSW-267
MCU+ SDK: SysConfig: Confusing "Initial Latency" settings for HYPERBUS PeripheralEXT_SITMPUSW-266
I2C Driver needs changes in I2C_transferEXT_SITMPUSW-265
Docs: ATF address is mentioned incorrectly for Falcon flowEXT_SITMPUSW-264
Incorrect size mentioned as comment in the MMCSD_RAW_IO source fileEXT_SITMPUSW-263
Design choice for Security Handover is not documentedEXT_SITMPUSW-262
mmcsd_raw_io_emmc_lld example is not workingEXT_SITMPUSW-261
AM275x FreeRTOS SDK: The CycleCounterP_getCount32 for R5F_0_0 is not accurateEXT_SITMPUSW-260
MCSPI Performance Numbers under MCU+ SDK documentation are not updatedEXT_SITMPUSW-259
eMMC retuning may be attempted during the initialization sequenceEXT_SITMPUSW-258
WKUP UART0 is not working in CallBack modeEXT_SITMPUSW-257
Roadmap for XIP Secure boot supportEXT_SITMPUSW-256
Incorrect calculation of rowColEnd in the ext_otp_writeMmrEXT_SITMPUSW-255
Sciclient driver uses incorrect context for TISCI_MSG_OPEN_DEBUG_FWLSEXT_SITMPUSW-254
Import from json does not workEXT_SITMPUSW-253
Sciclient driver uses incorrect context for Crypto TISCI APIsEXT_SITMPUSW-252
AM62X : Loading an A53 example is not working after the CPU Reset from the CCSEXT_SITMPUSW-251
MCU+ SDK Example Projects using incorrect ARMv7 MPU Attributes for Peripheral Register RegionEXT_SITMPUSW-250
AM62L: time: Application crashes due to time() functionEXT_SITMPUSW-249
2 C7x cores ( c7x_0 and c7x_1 ) in AM275 are not able to run 2 different McASP instancesEXT_SITMPUSW-246
AM62A : MCSPI DMA channels Teardown Failures When DMA transaction is Incomplete