Bootloader_socOpenFirewalls is called before System_init in the SBLs

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • SITSW-7462
    • 11.00.00
    • 12.00.00
    • Hide
      am62xx-sk
      am62xx-sk-lp
      am62x-sip-sk
      am62a-sk
      am62p-sk
      am62d-evm
      am275x-evm
      Show
      am62xx-sk am62xx-sk-lp am62x-sip-sk am62a-sk am62p-sk am62d-evm am275x-evm

      The `Bootloader_socOpenFirewalls` function call relies on the Sciclient driver for sending the TISCI messages. As such, the sciclient driver must be in initialized state before using it. This sciclient driver initialization happens as part of the System_init so the `Bootloader_socOpenFirewalls` function can not be called before System_init.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-6511 - Bootloader_socOpenFirewalls is call...
                SYNCHRONIZED
                • Last Sync Date: