AM62X : Loading an A53 example is not working after the CPU Reset from the CCS

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: High
    • SITSW-9216
    • CCS_20.4.0
    • Generic

      Please try the steps below to reproduce the issue.
      Load any A53 example from CCS
      Run it
      Pause it
      Do CPU Reset
      Load same example
      Here, the A53 core is not responding.
      Sometimes it goes to the hang in aborts and sometimes waiting for the semaphore signals for the UART .

      I have not fully spent time on this, but customers are expecting smooth loading an example of CCS for A53 core. It is similar to loading the R5F and M4F examples from CCS .

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-6228 - AM62X : Loading an A53 example is n...
                SYNCHRONIZED
                • Last Sync Date: