AM273x: ENET: TCP Server example needs second reset to successfully run the application

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium
    • SITSW-8086
    • 09.02.00
    • 13.01.00
    • am273x-evm

      https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1560887/am2732-about-qspi-boot-for-multi-core-application-image/6012466

      Issue Details:
      The investigation revealed that the issue did not originate from the multi-core image boot,
      Rather from a failure to initialise the PHY during the TCP server startup.
      The example used is enet_cpsw_tcpserver_am273x-evm_r5fss0-0_freertos_ti-arm-clang.

      From the UART logs, at power-on and when the reset button was pressed:
      On the first boot - Example fails
      After board reset - It works

      SDK version - 09.02.00.52
      Evaluation board - TMDS273EVM
      Example used - C:\ti\mcu_plus_sdk_am273x_09_02_00_52\examples\networking\lwip\enet_cpsw_tcpserver is imported into CCS and built. The application runs solely on CPU0.
      The issue still occurs even when running solely on CPU0.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-6269 - AM273x: ENET: TCP Server example ne...
                SYNCHRONIZED
                • Last Sync Date: