AASRC driver bug: AASRC_MAX_OUT_FIFO_THRESHOLD set to 16U

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • SITSW-9929
    • 11.02.00
    • 12.00.00
    • am275x-evm

      In source/drivers/aasrc/v0/aasrc_ch.h  -> line 75

      AASRC_MAX_OUT_FIFO_THRESHOLD macto is set to 16U, which should probably be 32U.
      In sysconfig also it allows a value upto 32. But when 32 is selected in sysconfig it fails without any error log due to this. 

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-6392 - AASRC driver bug: AASRC_MAX_OUT_FIF...
                SYNCHRONIZED
                • Last Sync Date: