Build failure with networking examples from mcu_plus_sdk inside ind_comms_sdk

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • SITSW-7945
    • Hide
      09.02.00
      09.00.00
      09.01.00
      Show
      09.02.00 09.00.00 09.01.00
    • 11.02.00
    • Hide
      am243x-lp
      am64xx-evm
      Show
      am243x-lp am64xx-evm
    • Hide
      If you're using an older version of the Industrial Communications SDK (prior to 2025_00_00_08), the following workaround can be used to successfully build Networking examples from MCU+ SDK using CCS projects:
      - Import the project into CCS
      - Create a backup of your .project file before making any changes
      - Open the .project file in a text editor
      - Locate all instances of COM_TI_INDUSTRIAL_COMMUNICATIONS_SDK_AM261X_INSTALL_DIR/mcu_plus_sdk in the locationURI attributes
      - Replace them with MCU_PLUS_SDK_PATH
      - Save the file and rebuild the project in CCS
      After implementing these changes, all linked files will be properly resolved, allowing the project to build successfully in CCS.
      Show
      If you're using an older version of the Industrial Communications SDK (prior to 2025_00_00_08), the following workaround can be used to successfully build Networking examples from MCU+ SDK using CCS projects: - Import the project into CCS - Create a backup of your .project file before making any changes - Open the .project file in a text editor - Locate all instances of COM_TI_INDUSTRIAL_COMMUNICATIONS_SDK_AM261X_INSTALL_DIR/mcu_plus_sdk in the locationURI attributes - Replace them with MCU_PLUS_SDK_PATH - Save the file and rebuild the project in CCS After implementing these changes, all linked files will be properly resolved, allowing the project to build successfully in CCS.

      On importing a networking example from mcu_plus_sdk packaged inside ind_comms_sdk, an error pops up once the project import completes stating: An internal error occured during: "Refreshing built-in compiler settings"

      Beyond this, operations such as build, clean, rebuild fail with the above error and the build error below: 

            • Clean-only build of configuration Debug for project enet_l2_cpsw_am64x-evm_r5fss0-0_freertos_ti-arm-clang ****

      "C:\\ti\\ccs1270\\ccs
      utils
      bin
      gmake" -k -j 20 clean -O 
       __ 
      gmake: *** No rule to make target 'clean'.

            • Build Finished ****

      The same issue is seen with all versions of ICSDK but the build using gmake works and the generated .out can be successfully loaded.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-6261 - Build failure with networking examp...
                SYNCHRONIZED
                • Last Sync Date: