Export - CSV (All fields)
Export - CSV (Current fields)
- EXT_EP-7591
pow(2,x) has fairly significant rounding error - EXT_EP-7705
DWARF does not correctly represent variables stored in register pairs - EXT_EP-7722
Extern inline functions are not supported in the C/C++ Compiler with COFF ABI - EXT_EP-7757
C2000 can't print 0 with %a format - EXT_EP-7763
strcmp doesn't correctly handle values with uppermost bit set - EXT_EP-7767
hex2000, while using -b option, mistakenly states a section "falls in unconfigured memory" - EXT_EP-7800
Forward reference in .space generates an internal error - EXT_EP-7829
printf gives wrong value for pointer when its value is incremented - EXT_EP-7897
C2000 RTS float arithmetic functions do not round correctly - EXT_EP-7954
C2000 float software multiply doesn't handle -1*INF properly - EXT_EP-8006
Linker gives misleading warning when dot expressions used in SECTION directive for .stack section - EXT_EP-8023
Structure is not initialized correctly when using -o2 or -o3 optimization - EXT_EP-8119
C2000 Assembler MACF32 pipeline detection error - EXT_EP-8142
Hex utility TI-tagged output has extra COFFTOTI string at the end of every line - EXT_EP-8149
_defs.h generates warning "shift count is too large" - EXT_EP-8170
Mistakenly including a C++ header file in C yields "Incompatible Redefinition" warning - EXT_EP-8550
error with using constexpr for return from end() with empty std::initializer_list - EXT_EP-8551
wostringstream::fill(WCHAR_MAX) incorrectly sets the fill value to ' 'L. - EXT_EP-8580
libcxx/include/random uses unsigned for unsigned long - EXT_EP-8582
noexcept(typeid(d)) runtime fail on polymorphic class type - EXT_EP-8583
deeply nested lambda functions causes a hang in the code generator - EXT_EP-8585
No error generated for lambda-expression in default argument cannot capture any entity. - EXT_EP-8587
TI compiler does not emit "error: constexpr function never produces a constant expression" - EXT_EP-8589
<regex> never throws error_ctype - EXT_EP-8712
Unimplemented core issue 1769: Catching a thrown derived class by reference to base clas - EXT_EP-8720
cannot find matching "==" operator definition - EXT_EP-8723
user-supplied allocator function is not called - EXT_EP-8727
Composing operations for valarray may fail to compile - EXT_EP-8730
Exception propagating out of noexcept function does not call std::terminate - EXT_EP-8731
std::linear_congruential_engine doesn't support 8-bit results - EXT_EP-8733
libcxx istreambuf_iterator points to end of string instead of character past match - EXT_EP-8737
Multiple non-variables may be declared using auto or decltype(auto) - EXT_EP-8745
cerr.tie() returns the wrong value - EXT_EP-8748
Initializing unordered_map with an initializer_list fails with -o2 or higher - EXT_EP-8749
1 ULP rounding error in double addition - EXT_EP-8752
Compiler aborts with excessive inlining of C++ functions - EXT_EP-8756
Internal error when passing a temporary array of objects - EXT_EP-8757
Cannot take the address of std::ctype<char>::table_size - EXT_EP-8758
Undefined symbol isblank with -g or -ooff - EXT_EP-8759
wstring runtime failure - likely bug in swprintf - EXT_EP-8760
Unexpected type returned by bitset [] operator - EXT_EP-8762
std::multimap::clear is not noexcept - EXT_EP-8766
regex_constants::ECMAScript not expected to be 0 - EXT_EP-8767
armcl allows non-default arguments to be specified after default arguments - EXT_EP-8768
Internal error when assigning default arguments to a parameter pack - EXT_EP-8770
Failure to defer C++ access control checks - EXT_EP-8771
decltype cannot be used as a destructor name - EXT_EP-8772
Unimplemented core issue 475: std::uncaught_exception is not true when constructing the thrown object - EXT_EP-8826
std::num_get does not parse floating-point strings correctly - EXT_EP-8990
Using --gen_profile_info with code with CLA source fails to build
{"errorMessages":["jqlTooComplex"],"errors":{}}
[{"id":-1,"name":"My open issues","jql":"assignee = currentUser() AND resolution = Unresolved order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":true},{"id":-2,"name":"Reported by me","jql":"reporter = currentUser() order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":true},{"id":-4,"name":"All issues","jql":"order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-5,"name":"Open issues","jql":"resolution = Unresolved order by priority DESC,updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-9,"name":"Done issues","jql":"statusCategory = Done order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-3,"name":"Viewed recently","jql":"issuekey in issueHistory() order by lastViewed DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-6,"name":"Created recently","jql":"created >= -1w order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-7,"name":"Resolved recently","jql":"resolutiondate >= -1w order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-8,"name":"Updated recently","jql":"updated >= -1w order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false}]
0.3
0