cannot find matching "==" operator definition

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Low
    • Code Generation Tools
    • CODEGEN-4132
    • Hide
      ARM_18.1.0.LTS
      MSP430_18.1.0.LTS
      C2000_22.6.0.LTS
      MSP430_20.2.0.LTS
      C2000_25.11.0.LTS
      ARM_18.12.0.LTS
      MSP430_21.6.0.LTS
      C2000_21.6.0.LTS
      MSP430_18.12.0.LTS
      ARM_20.2.0.LTS
      Show
      ARM_18.1.0.LTS MSP430_18.1.0.LTS C2000_22.6.0.LTS MSP430_20.2.0.LTS C2000_25.11.0.LTS ARM_18.12.0.LTS MSP430_21.6.0.LTS C2000_21.6.0.LTS MSP430_18.12.0.LTS ARM_20.2.0.LTS
    • Hide
      The library does not provide an definition of std::operator== for arguments of type std::istream_iterator. That is, the following code is erroneously marked as ill-formed with a diagnostic:

      #include <iterator>
      #include <string>
      using ISTREAM_ITER_C = std::istream_iterator<char, char>;

      bool foo(const ISTREAM_ITER_C& arg00 ,const ISTREAM_ITER_C& arg01 ){
      return std::operator== (arg00, arg01); // Syntax error
      }

      However, this is only an issue if called in exactly that way. Using it as an operator, rather than as a function call, works as expected:

      arg00 == arg01 // Works
      Show
      The library does not provide an definition of std::operator== for arguments of type std::istream_iterator. That is, the following code is erroneously marked as ill-formed with a diagnostic: #include <iterator> #include <string> using ISTREAM_ITER_C = std::istream_iterator<char, char>; bool foo(const ISTREAM_ITER_C& arg00 ,const ISTREAM_ITER_C& arg01 ){ return std::operator== (arg00, arg01); // Syntax error } However, this is only an issue if called in exactly that way. Using it as an operator, rather than as a function call, works as expected: arg00 == arg01 // Works

      cannot find matching "==" operator definition

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-1223 - cannot find matching "==" operator ...
                SYNCHRONIZED
                • Last Sync Date: