DWARF does not correctly represent variables stored in register pairs

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Low
    • Code Generation Tools
    • CODEGEN-63
    • SDSCM00008685
    • Hide
      C2000_16.9.0.LTS
      MSP430_21.6.0.LTS
      C6000_8.1.0B1
      C6000_7.4.0B1
      ARM_5.2.0B1
      MSP430_16.9.0.LTS
      ARM_15.12.0.LTS
      C6000_8.2.0
      C2000_18.1.0.LTS
      C2000_6.4.0B1
      C6000_8.3.0
      MSP430_20.2.0.LTS
      ARM_18.12.0.LTS
      C2000_21.6.0.LTS
      MSP430_15.12.0.LTS
      ARM_20.2.0.LTS
      C2000_20.2.0.LTS
      ARM_18.1.0.LTS
      MSP430_18.1.0.LTS
      ARM_16.9.0.LTS
      C2000_22.6.0.LTS
      C2000_25.11.0.LTS
      C2000_15.12.0.LTS
      MSP430_4.4.0B1
      MSP430_18.12.0.LTS
      C2000_18.12.0.LTS
      Show
      C2000_16.9.0.LTS MSP430_21.6.0.LTS C6000_8.1.0B1 C6000_7.4.0B1 ARM_5.2.0B1 MSP430_16.9.0.LTS ARM_15.12.0.LTS C6000_8.2.0 C2000_18.1.0.LTS C2000_6.4.0B1 C6000_8.3.0 MSP430_20.2.0.LTS ARM_18.12.0.LTS C2000_21.6.0.LTS MSP430_15.12.0.LTS ARM_20.2.0.LTS C2000_20.2.0.LTS ARM_18.1.0.LTS MSP430_18.1.0.LTS ARM_16.9.0.LTS C2000_22.6.0.LTS C2000_25.11.0.LTS C2000_15.12.0.LTS MSP430_4.4.0B1 MSP430_18.12.0.LTS C2000_18.12.0.LTS
    • Hide

      Although 'var1' and 'var2' are shown to be in single registers, a
      debugger could determine that they are actually stored in register
      pairs by looking at the type of the variables:

         [00000113] DW_TAG_base_type
          DW_AT_name long long
          DW_AT_encoding 0x5
          DW_AT_byte_size 0x8

      The base type indicates that the size of the variables is 0x8 bytes.
      Since a single register can only store 0x4 bytes of information, it
      would take two registers to hold this values.

      On TI architectures, values stored in multiple registers are always
      stored in consecutive registers. Thus, the debugger would know that
      if the entire value could not fit in A4, the rest of the value must be
      in A5. A5 would contain the upper 32 bits of the value.



      Show
      Although 'var1' and 'var2' are shown to be in single registers, a debugger could determine that they are actually stored in register pairs by looking at the type of the variables:    [00000113] DW_TAG_base_type     DW_AT_name long long     DW_AT_encoding 0x5     DW_AT_byte_size 0x8 The base type indicates that the size of the variables is 0x8 bytes. Since a single register can only store 0x4 bytes of information, it would take two registers to hold this values. On TI architectures, values stored in multiple registers are always stored in consecutive registers. Thus, the debugger would know that if the entire value could not fit in A4, the rest of the value must be in A5. A5 would contain the upper 32 bits of the value.

      DWARF does not correctly represent variables stored in register pairs

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-208 - DWARF does not correctly represent ...
                SYNCHRONIZED
                • Last Sync Date: