Extern inline functions are not supported in the C/C++ Compiler with COFF ABI

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Low
    • Code Generation Tools
    • CODEGEN-71
    • SDSCM00008928
    • Hide
      C2000_16.9.0.LTS
      C2000_18.1.0.LTS
      C2000_22.6.0.LTS
      C2000_6.4.0B1
      C2000_25.11.0.LTS
      C2000_15.12.0.LTS
      MSP430_4.4.0B1
      C2000_21.6.0.LTS
      C6000_7.4.0B1
      ARM_5.2.0B1
      C2000_18.12.0.LTS
      C2000_20.2.0.LTS
      Show
      C2000_16.9.0.LTS C2000_18.1.0.LTS C2000_22.6.0.LTS C2000_6.4.0B1 C2000_25.11.0.LTS C2000_15.12.0.LTS MSP430_4.4.0B1 C2000_21.6.0.LTS C6000_7.4.0B1 ARM_5.2.0B1 C2000_18.12.0.LTS C2000_20.2.0.LTS
    • This bug only affects COFF ABI. If a function is declared as inline and there are no references to it in the same file, the function is eliminated and can't be called from another file.

      Extern inline functions are not supported in the C/C++ Compiler with COFF ABI

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-225 - Extern inline functions are not sup...
                SYNCHRONIZED
                • Last Sync Date: