Using --gen_profile_info with code with CLA source fails to build

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Low
    • Code Generation Tools
    • CODEGEN-4960
    • Hide
      C2000_22.6.0.LTS
      C2000_25.11.0.LTS
      C2000_18.1.2.LTS
      C2000_21.6.0.LTS
      C2000_18.12.0.LTS
      C2000_20.2.0.LTS
      Show
      C2000_22.6.0.LTS C2000_25.11.0.LTS C2000_18.1.2.LTS C2000_21.6.0.LTS C2000_18.12.0.LTS C2000_20.2.0.LTS
    • N/A.
    • Hide
      As the title says, when using the --gen_profile_info option with a project that contains CLA code, it fails with an invalid filename as shown in the error message below:

      >> Compilation failure
      subdir_rules.mk:58: recipe for target 'matrix_mpy.obj' failed
      fatal error: Error opening icode file
      "C:\\Users\\user\\AppData\\Local
      Temp

      {B38860D0-28F1-4B19-9A99-2F0EA95 A0EA8}
      ":
      >> Abort - Cannot open input icode file C:\\Users\\user\\AppData\\Local\\Temp\\\\

      {B38860D0-28F1-4B19-9A99-2F0EA95A0EA8}
      p: No such file or directory

      This does not happen with F28x projects that are free of CLA code.

      This was reproduced in CCSv8.1.0 with the default C2000 compiler version 18.1.2

      No plans to address at this time.
      Show
      As the title says, when using the --gen_profile_info option with a project that contains CLA code, it fails with an invalid filename as shown in the error message below: >> Compilation failure subdir_rules.mk:58: recipe for target 'matrix_mpy.obj' failed fatal error: Error opening icode file "C:\\Users\\user\\AppData\\Local Temp {B38860D0-28F1-4B19-9A99-2F0EA95 A0EA8} ": >> Abort - Cannot open input icode file C:\\Users\\user\\AppData\\Local\\Temp\\\\ {B38860D0-28F1-4B19-9A99-2F0EA95A0EA8} p: No such file or directory This does not happen with F28x projects that are free of CLA code. This was reproduced in CCSv8.1.0 with the default C2000 compiler version 18.1.2 No plans to address at this time.

      Using --gen_profile_info with code with CLA source fails to build

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-1493 - Using --gen_profile_info with code ...
                SYNCHRONIZED
                • Last Sync Date: