user-supplied allocator function is not called

XMLWordPrintable

    • Type: Bug
    • Resolution: Cannot Reproduce
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-4119
    • Hide
      ARM_18.1.0.LTS
      MSP430_18.1.0.LTS
      C2000_22.6.0.LTS
      MSP430_20.2.0.LTS
      C2000_25.11.0.LTS
      ARM_18.12.0.LTS
      MSP430_21.6.0.LTS
      C2000_21.6.0.LTS
      MSP430_18.12.0.LTS
      ARM_20.2.0.LTS
      Show
      ARM_18.1.0.LTS MSP430_18.1.0.LTS C2000_22.6.0.LTS MSP430_20.2.0.LTS C2000_25.11.0.LTS ARM_18.12.0.LTS MSP430_21.6.0.LTS C2000_21.6.0.LTS MSP430_18.12.0.LTS ARM_20.2.0.LTS
    • C7000_NEXT
    • I cannot reproduce on main tools and I cannot reproduce with old tools. Either this item is bogus or potentially the issue could have been an error in Perennial C++ which we have since upgraded past.

      A user-supplied allocator function is not called.

      The test checks to make sure that a user-supplied allocator function is actually called during the construction of a unordered_multiset object where one of the template parameters is the pointer to the user-supplied allocator function.

      While at least some of the unordered_multiset constructor functions appear to utilize the user-supplied allocator function, there are also some that do not and in this particular test, one of the constructors that does not call the user-supplied allocator function is called. The test is monitoring whether or not the user-supplied allocator function gets called via a global flag, and since the allocator function is not called, the test fails.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-1226 - user-supplied allocator function is...
                SYNCHRONIZED
                • Last Sync Date: