- EXT_EP-12339Switch/MAC/HSR firmware does not drop corrupted packets
- EXT_EP-11975Connection param and channel map update call backs are coming earlier than the actual instant where the change is reflected in the connection causing CM instability
- EXT_EP-10713Long duration run of vision apps tidl object detection demo hangs at high usage of A72
- EXT_EP-11770[SPS] BLE Stack supports Periodic Extended Advertising
- EXT_EP-7567add llEnter/llExit around calls to SockCleanPcb()
- EXT_EP-9120Support the SimpleLink 2.30 (Q3 2018) SDKs
- EXT_EP-9121Update to October 2018 LTS release
- EXT_EP-9125Support the SimpleLink 2.30 (Q3 2018) SDKs
- EXT_EP-9144Support the SimpleLink 2.40 (Q4 2018) SDKs
- EXT_EP-9177Support the SimpleLink 2.40 (Q4 2018) SDKs
- EXT_EP-9179Support the SimpleLink 2.40 (Q4 2018) SDKs
- EXT_EP-9422Support the SimpleLink 3.20 (Q2 2019) SDKs
- EXT_EP-9546Support the SimpleLink 3.30 (Q3 2019) SDKs
- EXT_EP-9583Support the SimpleLink 3.30 (Q3 2019) SDKs
- EXT_EP-12336Last 1B of payload missing in forwarding scenario
- EXT_EP-12297Project Wizard loses connection when specific boards or devices are selected (F28P55x)
- EXT_EP-12207Project wizard fails when looking for examples for F28P55x
- EXT_EP-12355For large watch expression arrays, we fetch all values instead of what is visible
- EXT_EP-10678IPC Performance Test hangs after loading the binary
- EXT_EP-12043TPS6594: Error IRQ trap reach ilim, overcurrent for
- EXT_EP-12350RCU Torture test results in a crash
- EXT_EP-12264CCS Server crash prevents saving of workspace files
- EXT_EP-12345beagleplay: Segmentation-Fault: SD Boot failure and needs bootcmd update
- EXT_EP-12341Linux: AM62-LP-SK: SDK 11 Deep Sleep is non-functional
- EXT_EP-12340Suspend-to-RAM failure: tps65219: device creates a circular dependency and device fails to enter suspend
- EXT_EP-12337ICSSG: TAPRIO - Firmware can’t handle base-time which is not a multiple of cycle-time.
- EXT_EP-12278ECC Aggregator SMS0_SMS_HSM_ECC Aggr fails on AM62x
- EXT_EP-12280Running MCU LBIST on SBL causes JTAG connection issues to MCU R5F
- EXT_EP-12314MJPEG Encoding doesn't work for 5MP resolution - 2592x1952.
- EXT_EP-12178sdl:j721e PG2.0: PBIST unit test and functional test is failing for HC instance
- EXT_EP-12301DSS causes a freeze of processes every 10 seconds for about 200ms
- EXT_EP-12296AM62x: 6.12 LTS Regression: PRU IPC Failure due to driver missing
- EXT_EP-12292Cannot import examples or download SDKs from Resource Explorer
- EXT_EP-12231Symbol auto completion for debug views
- EXT_EP-12142Instabilities observed while resuming from IO Only plus DDR mode
- EXT_EP-12213clock() causes an illegal memory access
- EXT_EP-12253If MC 'start_task' request to a spawner fails, MC believes the session started and blocks the user from starting train sessions
- EXT_EP-12157Exception can occur running downloaded ccs_setup executable during incremental update.
- EXT_EP-12226Linux SDK v10.0: U-Boot "go" command needs Linux Kernel-like cache/MMU cleanup so 3rd Party OS can startup correctly
- EXT_EP-11238UniFlash CLI: dslite does not return on failure when programming a Cortex M3
- EXT_EP-12205SK-AM68 intermittently fails to boot on warm reset
- EXT_EP-12017Getting started actions that use localID links do not work
- EXT_EP-11659[SWAT] Scanner failes after receiving an incorrect event type
- EXT_EP-12183When there are two ADV with different RPAs generating from the same IRK, CC2642 can hardly scan the ADVs
- EXT_EP-12160Can't Delete Images Unless They Are Selected
- EXT_EP-10730[MESH][AE][eRPC] ~100% missing packets more than 3 hops while GATT Bearer is enabled
- EXT_EP-12079AM335x: UART and GPIO Wakeup from Standby Failed
- EXT_EP-12067AM335x/AM437x PRU Ethernet slowdown from kernel 4.19 -> 5.4/5.10
- EXT_EP-12037J784s4: WKUP_UART as console hangs in R5 SPL in SDK 10.0
- EXT_EP-12019Sciclient service secure proxy fails in AUTOSAR OS context
1 of 2570