beagleplay: Segmentation-Fault: SD Boot failure and needs bootcmd update

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • Linux Core SDK
    • LCPD-43466
    • 11.00
    • 11.02
    • beagleplay-gp

      root@beagleplay-ti:~# /usr/share/examples/opengl/hellogles3/bin/hellogles3 -platform eglfs
      Detected locale "C" with character encoding "ANSI_X3.4-1968", which is not UTF-8.
      Qt depends on a UTF-8 locale, and has switched to "C.UTF-8" instead.
      If this causes problems, reconfigure your locale. See the locale(1) manual
      for more information.
      Failed to move cursor on screen HDMI1: -13
      Failed to move cursor on screen HDMI1: -13
      Requesting 3.0 context
      libEGL warning: DRI2: failed to rebind the previous context[ 109.147142] audit: type=1701 audit(1736362013.396:36): auid=4294967295 uid=0 gid=0 ses=4294967295 subj=kernel pid=1167 comm="hellogles3" exe="
      /usr/share/examples/opengl/hellogles3/bin/hellogles3" sig=11 res=1
      QEGLPlatformContext: eglMakeCurrent failed: 3009
      QOpenGLWindo[ 109.165154] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000018
      w::beginPaint: Failed to make context current
      [ 109.184778] Mem abort info:
      [ 109.191496] ESR = 0x0000000096000006
      [ 109.195252] EC = 0x25: DABT (current EL), IL = 32 bits
      [ 109.200562] SET = 0, FnV = 0
      [ 109.203627] EA = 0, S1PTW = 0
      [ 109.206768] FSC = 0x06: level 2 translation fault
      [ 109.211647] Data abort info:
      [ 109.214534] ISV = 0, ISS = 0x00000006, ISS2 = 0x00000000
      [ 109.220053] CM = 0, WnR = 0, TnD = 0, TagAccess = 0
      [ 109.225103] GCS = 0, Overlay = 0, DirtyBit = 0, Xs = 0
      [ 109.230433] user pgtable: 4k pages, 48-bit VAs, pgdp=0000000084c78000
      [ 109.236872] [0000000000000018] pgd=0800000082d44003, p4d=0800000082d44003, pud=08000000a383c003, pmd=0000000000000000
      [ 109.247496] Internal error: Oops: 0000000096000006 3 PREEMPT SMP
      [ 109.253751] Modules linked in: wl18xx wlcore mac80211 libarc4 snd_soc_hdmi_codec pru_rproc irq_pruss_intc cc33xx_sdio snd_soc_simple_card crct10dif_ce wlcore_sdio snd_soc_simple_card_utils pvrsrvkm(O)
      display_connector overlay rti_wdt k3_j72xx_bandgap tidss rtc_ti_k3 drm_dma_helper snd_soc_davinci_mcasp snd_soc_ti_udma snd_soc_ti_edma sa2ul mcrc64 pruss snd_soc_ti_sdma drm_display_helper cfg80211 ite_i
      t66121 omap_hwspinlock omap_mailbox tps65219_pwrbutton drm_kms_helper rtc_bq32k at24 spi_omap2_mcspi pwm_tiecap ramoops reed_solomon bluetooth ecdh_generic ecc rfkill cryptodev(O) fuse drm drm_panel_orien
      tation_quirks backlight ipv6
      [ 109.309612] CPU: 0 UID: 0 PID: 1169 Comm: systemd-coredum Tainted: G D O 6.12.17-ti-00771-gc85877d40f8e #1
      [ 109.320470] Tainted: [D]=DIE, [O]=OOT_MODULE
      [ 109.324729] Hardware name: beagle BeagleBoard.org BeaglePlay/BeagleBoard.org BeaglePlay, BIOS 2025.01-00406-gcd91d7360181 01/01/2025
      [ 109.336616] pstate: 80000005 (Nzcv daif PAN -UAO -TCO -DIT -SSBS BTYPE=-)
      [ 109.343570] pc : pvr_show_fdinfo+0x90/0xd4 [pvrsrvkm]
      [ 109.348875] lr : seq_show+0x160/0x234
      [ 109.352545] sp : ffff80008802bb40
      [ 109.355850] x29: ffff80008802bbb0 x28: ffff000003628560 x27: 0000000000400cc0
      [ 109.362986] x26: ffff000006298e40 x25: ffff000008024960 x24: 0000000000000000
      [ 109.370115] x23: ffff000006298dc0 x22: 00000000000a0002 x21: ffff000003628528
      [ 109.377243] x20: ffff000002e93000 x19: ffff000003628528 x18: ffffffffffffffff
      [ 109.384374] x17: 0000000000000000 x16: 0000000000000000 x15: ffff80008802ba20
      [ 109.391500] x14: 0000000000000000 x13: ffff000001a36027 x12: 0000000000000000
      [ 109.398628] x11: 0000000000000000 x10: 000000000000000a x9 : 0000000000000198
      [ 109.405755] x8 : 000000000000000a x7 : 0000000000000000 x6 : 0000000000000000
      [ 109.412883] x5 : ffff000003849700 x4 : 0000000000000000 x3 : 000000000000048f
      [ 109.420012] x2 : ffff000004b88000 x1 : ffff80008802bb48 x0 : ffff8000799949ac
      [ 109.427142] Call trace:
      [ 109.429581] pvr_show_fdinfo+0x90/0xd4 [pvrsrvkm]
      [ 109.434411] seq_show+0x160/0x234
      [ 109.437722] seq_read_iter+0xe0/0x454
      [ 109.441384] seq_read+0xf0/0x138
      [ 109.444608] vfs_read+0xc4/0x320
      [ 109.447832] ksys_read+0x74/0x10c
      [ 109.451141] __arm64_sys_read+0x1c/0x28
      [ 109.454971] invoke_syscall+0x48/0x10c
      [ 109.458724] el0_svc_common.constprop.0+0xc0/0xe0
      [ 109.463422] do_el0_svc+0x1c/0x28
      [ 109.466732] el0_svc+0x28/0x98
      [ 109.469784] el0t_64_sync_handler+0x120/0x12c
      [ 109.474134] el0t_64_sync+0x190/0x194
      [ 109.477798] Code: f9401c85 f9404c44 f94000a2 b9407063 (b9401884)
      [ 109.483884] --[ end trace 0000000000000000 ]--
      Segmentation fault (core dumped)

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-5325 - beagleplay: Segmentation-Fault: SD ...
                SYNCHRONIZED
                • Last Sync Date: