Export - CSV (All fields)
Export - CSV (Current fields)
EXT_SITMPUSW-40
The SYSFW_IMAGE_INTEGRITY OID is incorrectly mentioned in the commentEXT_SITMPUSW-39
Error in the CCS build of the SBL examplesEXT_SITMPUSW-38
Remote core getting hangs when doing IPC with HLOSEXT_SITMPUSW-37
Misleading "File read from SD card" bootloader profile point in the SBL_SD bootloaderEXT_SITMPUSW-36
MMCSD_initSD does not check the retry variable for failure for OCR commandEXT_SITMPUSW-35
MMCSD_initSD always returns SUCCESSEXT_SITMPUSW-34
SBL_UART_UNIFLASH_STAGE2 build fails on removing OSPI and FLASH module in SysconfigEXT_SITMPUSW-33
Resolve GPU crash caused by Display cluster demoEXT_SITMPUSW-32
SDK Makefile: Fix logic to pick key directory for mkimageEXT_SITMPUSW-31
IPC Firmwares missing from base images.EXT_SITMPUSW-30
Debian: Deepsleep doesn't work on AM62PEXT_SITMPUSW-29
TI Debian SDK: Docker not workingEXT_SITMPUSW-28
Outstanding mailbox messages prevent suspendEXT_SITMPUSW-27
gmake when run from windows command prompt with -j can sometimes lock up the command promptEXT_SITMPUSW-26
AM64X PCIe MSI error when connected to Linux Root ComplexEXT_SITMPUSW-25
AM243x/AM64x: last 512KB of memory is not accessible in dev boot mode flowEXT_SITMPUSW-24
[SA2UL][PKA] ECDSA Sign/verify not working with P-521 and BrainPool P-512R1 CurvesEXT_SITMPUSW-23
[Docs] Sysfw RM/PM documentation doesn't specify AM243xEXT_SITMPUSW-22
Pcie_benchmark, Pcie_buf_transfer, Pcie_legacy_irq, Pcie_msi_irq and Pcie_msix_irq are broken on 9.2.1 releaseEXT_SITMPUSW-21
DMA not working with ADC FIFO 1EXT_SITMPUSW-20
No implementation for portASSERT_IF_IN_ISREXT_SITMPUSW-19
Not able to open drivers for MCU_I2CEXT_SITMPUSW-18
sciclient_ccs_init default binary failing to run on SOCEXT_SITMPUSW-17
Not able to open example.syscfg file for M4f projectEXT_SITMPUSW-16
Not able to select 3pin/4pin mode when mcspi is configured as Single PeripheralEXT_SITMPUSW-15
Wrong validation checks for Sysfw_boardcfgEXT_SITMPUSW-14
JTAG Flasher does not enable DAC mode after flashing the imageEXT_SITMPUSW-13
UART: Inconsistent data flush for Polling, Interrupt and DMA modeEXT_SITMPUSW-12
A wrong counter is used for Event 2 in PMU configurationEXT_SITMPUSW-11
MCAN loopback DMA example is brokenEXT_SITMPUSW-10
SBL_OSPI_LINUX changes the DEVSTAT register to SD card bootmodeEXT_SITMPUSW-9
Calling the vTaskGetRunTimeStats,after some time, it will exceed 100% CPU usageEXT_SITMPUSW-8
Remove "Auto generated makefile" comments in the makefilesEXT_SITMPUSW-7
OSPI_phyReadAttackVector API leaves the DAC enabledEXT_SITMPUSW-6
Incorrect naming of the macro MAILBOX_MAX_MSGS_IN_FIFO in IPC NotifyEXT_SITMPUSW-5
Potential Infinite loop in OSPI_utilLog2 defined in ospi_v0.cEXT_SITMPUSW-3
EMMC:The tuning algorithm to re-execute up to 10 times if there is no failing or passing itapdly.EXT_SITMPUSW-2
Generated tiboot3.bin in SBL examples are copy of GP images instead of HSFSEXT_SITMPUSW-1
CPU cache line size is wrongly documentedEXT_PSDKQA-29
TDA4VM: Duplication of messages received by RPMessage_recv()EXT_PSDKQA-28
QNX IPC - Need to make the task priority a configurable item.EXT_PSDKQA-27
Remove DEBUG_PRINT flag in the ipclld common.mk fileEXT_PSDKQA-25
OSAL: DebugP_log1 using _SLOG_ERROR instead of _SLOG_LOGEXT_PSDKQA-24
SDK to evaluate and remove short_enums compiler flag across modulesEXT_PSDKQA-23
Address Compiler Warning -Wno-address-of-packed-memberEXT_PSDKQA-22
SafeRTOS: IPC echo test fails to ping mcu coresEXT_PSDKQA-21
[IPC]: RPMessage_recv sometimes returns SOK with no dataEXT_PSDKQA-20
J721S2: MCU-CPSW non-functional when using SBL bootloaderEXT_PSDKQA-19
J722S: Cache invalidate on A53 inconsistent for remoteproc use casesEXT_PSDKQA-18
CPSW5G/9G: Destroying interface freezes prompt