J722S: Cache invalidate on A53 inconsistent for remoteproc use cases

XMLWordPrintable

    • Type: Bug
    • Resolution: Won't Fix
    • Priority: High
    • Processor SDK QNX
    • PSDKQA-1718
    • Hide
      PSDKQA_10.0
      PSDKQA_9.2
      Show
      PSDKQA_10.0 PSDKQA_9.2
    • PSDKQA_9.2
    • j722s-evm
    • This was found to be a framework issue and not a QNX issue

      On J722S, when testing with Vision apps conformance tests, we see that the cache invalidate calls on the A53 cores does not seem to have the desired effect. The memory range that the cache invalidate operates on seems to have stale data.

      Other observations:

      • When the memory region is marked non-cached on the A53 side, the issue is not seen, but the performance deteriorates severely.
      • This issue is seen when exchanging buffers between C7x and A53.
      • This issue is seen on Sitara devices also.
      • This issue is only seen for QNX HLOS.

       

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4533 - J722S: Cache invalidate on A53 inco...
                SYNCHRONIZED
                • Last Sync Date: