Not able to open drivers for MCU_I2C

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • SITSW-5389
    • 10.00.00
    • 10.01.00
    • Hide
      am243x-evm
      am243x-lp
      am64xx-evm
      am64xx-sk
      Show
      am243x-evm am243x-lp am64xx-evm am64xx-sk

      Configuring the MCU_I2C instance for R5F example is provided in the MCU+SDK.

      The build is successful but when trying to run the example, there is an error in I2C_open.

      ASSERT: 0.1043s: i2c/v0/i2c_v0.c: I2C_open:340: status==SystemP_SUCCESS failed !!!

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4938 - Not able to open drivers for MCU_I2C
                SYNCHRONIZED
                • Last Sync Date: