gmake when run from windows command prompt with -j can sometimes lock up the command prompt

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Not Prioritized
    • SITSW-6144
    • 07.03.00
    • This is a known issue in windows cmd prompt

      This is a windows limitation.

      Workarounds,

      This is not seen always.

      This issue is seen with library build only as well, so its not a sysconfig issue

      This isssue is not seen in Linux. This issue is not seen when using git bash for windows

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-4948 - gmake when run from windows command...
                SYNCHRONIZED
                • Last Sync Date: