Not able to select 3pin/4pin mode when mcspi is configured as Single Peripheral

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • SITSW-5113
    • 10.00.00
    • 10.01.00
    • Hide
      am243x-evm
      am243x-lp
      am64xx-evm
      am64xx-sk
      Show
      am243x-evm am243x-lp am64xx-evm am64xx-sk

      In the example.syscfg file when we are trying to configure the MCSPI peripheral in single Peripheral mode. The option to select pin mode(3Pin / 4Pin) is getting disappeared.

       

      Please refer below screenshot.

      Single Controller ->  works fine

      Single Peripheral  -> option not visible

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4935 - Not able to select 3pin/4pin mode w...
                SYNCHRONIZED
                • Last Sync Date: