Export - CSV (All fields)
Export - CSV (Current fields)
EXT_SITMPUSW-193
DMA is not enabled for SOC Memory boot media in the SysConfigEXT_SITMPUSW-192
SysConfig does not support configuring both 10-bit own addresses for I2C target modeEXT_SITMPUSW-191
I2C_transfer() return not handled properly while i2cLldHandle is NULLEXT_SITMPUSW-190
OSPI_PhyTuneGrapher missing read delay value 4EXT_SITMPUSW-189
Secure board configurations by default allows JTAG unlockingEXT_SITMPUSW-188
[MCSPI]End of Channel Transfer status check is missing for DMA modeEXT_SITMPUSW-187
OSPI DAC Mode Configuration hardcoded and not based on flashsizeEXT_SITMPUSW-186
MMCSD : Read fails when injecting Command CRC faultEXT_SITMPUSW-185
MMCSD : Read times out in HS200 mode after writing in SDR50 modeEXT_SITMPUSW-184
I2c bus is not available after recoveryEXT_SITMPUSW-183
I2c_transfer not returning correct status when transfer mode is set to pollingEXT_SITMPUSW-181
Configured dummy cycles in flash driver contradicts flash data sheetEXT_SITMPUSW-180
Mailbox maximum fifo messages count is incorrectEXT_SITMPUSW-179
I2C Target Overrun Test Hangs Waiting for CallbackEXT_SITMPUSW-178
Incorrect handling of the donedataLen in the SA2UL_contextProcessEXT_SITMPUSW-177
Invalid comment in the linker command filesEXT_SITMPUSW-176
MMCSD : Read fails when injecting Command Index faultEXT_SITMPUSW-175
AM62D: Fix vring allocation to work along with MCAL running on MCU-R5FEXT_SITMPUSW-174
UDMA: HC/UHC channel allocation fails due to RM config mismatch with CSL definesEXT_SITMPUSW-173
Incorrect calculation of ptrInput and ptrOutput in the SA2UL_contextProcessEXT_SITMPUSW-172
DebugP_assert: change so that it does not lock up the entire coreEXT_SITMPUSW-171
MMCSD : Read fails when injecting Command time out faultEXT_SITMPUSW-170
I2C_open returning invalid handle when lock failsEXT_SITMPUSW-169
C7x Minimum stack size is increased from 10.1 to 11.0 for AM62A, AM62DEXT_SITMPUSW-168
MCU+ SDK CCS Project Build Generates Invalid/Redundant Boot Image FilesEXT_SITMPUSW-167
SBL OSPI failing with large sized applicationEXT_SITMPUSW-166
ti-apps-launcher: Incomplete Demo Build stepsEXT_SITMPUSW-165
inapplicable wl18xx message in Linux boot logEXT_SITMPUSW-164
Missing IPC echo firmware / mismatched u-boot instructions for DM firmware nameEXT_SITMPUSW-163
k3conf utility is not packaged with Buildroot image.EXT_SITMPUSW-162
Sciclient, update the context ID check in sciclient ISREXT_SITMPUSW-161
Possibility of different sequence id initialization in a multi thread environmentEXT_SITMPUSW-160
RSA PSS signing in the appimage signing script is brokenEXT_SITMPUSW-159
SBL SD is broken on AM62PEXT_SITMPUSW-158
OSPI_flashExecCmd has a couple of checks where the code may get stuckEXT_SITMPUSW-157
gMemBootloaderConfig in the bootloader driver is not thread safeEXT_SITMPUSW-156
Sciserver: gSecHeaderSizeWords variable is not thread safeEXT_SITMPUSW-155
eMMC Driver Error Recovery Recursion can lead to System CrashesEXT_SITMPUSW-154
MSC ROI function not creating the desired ROIEXT_SITMPUSW-153
eMMC Driver Error Interrupt Flags accessed in Wrong RegisterEXT_SITMPUSW-152
Heterogeneous-camera streaming with imx390 followed by ov2312 gets stalled.EXT_SITMPUSW-151
VPAC switching between WDR mode and linear mode causing wrong image colorEXT_SITMPUSW-150
Drop edgeai override for AM62AEXT_SITMPUSW-149
AM62A: Display starvation observed while running Semantic Segmentation usecaseEXT_SITMPUSW-148
Relocate Memory carveout for RTOS IPCEXT_SITMPUSW-147
Multichannel demo in EdgeAI gallery freezes on long runEXT_SITMPUSW-146
Yocto: meta-ti*: kernel source has uncommited changesEXT_SITMPUSW-145
Linux SDK User Manual needs Customer-Accessible Change Log / Revision HistoryEXT_SITMPUSW-144
Multichannel EdgeAI pipeline - Multi Input Single Inference freezes on long runEXT_SITMPUSW-143
Yocto Documentation: AM6x: SDK: Build Instruction missing steps for building K3R5 baremetal toolchain