Sciclient, update the context ID check in sciclient ISR

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • SITSW-8061
    • 11.01.00
    • Hide
      11.01.01
      11.02.00
      Show
      11.01.01 11.02.00
    • Hide
      am62xx-sk
      am62a-sk
      am62p-sk
      Show
      am62xx-sk am62a-sk am62p-sk

      The context id check is not correct at the following place

      https://github.com/TexasInstruments/mcupsdk-core-k3/blob/k3_next/source/drivers/device_manager/sciclient_direct/sciclient.c#L1119-L1119

      The `contextId` variable is upper bounded by the macro SCICLIENT_CONTEXT_MAX_NUM. Not having this upper bound check could lead to array out of index accesses.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-6013 - Sciclient, update the context ID ch...
                SYNCHRONIZED
                • Last Sync Date: