Export - CSV (All fields)
Export - CSV (Current fields)
EXT_EP-9590
Compiler generates many more single cycle NOP instructionsEXT_EP-9565
Compiler computes wrong offset for structure member, causing CCS to display it incorrectlyEXT_EP-9609
Customer SA0ADV code crashes parserEXT_EP-9606
Calling array delete with null pointer causes hardware exception to occurEXT_EP-9572
Compiler fails with >> INTERNAL ERROR: >>>Register allocation failedEXT_EP-9779
Add RSA/EFI intrinsic handling back into C6000 compiler under --legacy optionEXT_EP-9776
#include <math.h> causes compiler to emit advice: (Performance) EABI double precision is 64-bits as opposed to 32-bits for COFFEXT_EP-9775
Customer requests option for all remarks as errorsEXT_EP-9780
Linker internal error when crc_table is applied to EXIDXEXT_EP-9746
Compiler fails with INTERNAL ERROR: ac2000 experienced a segmentation faultEXT_EP-9786
In the map file MEMORY CONFIGURATION table, the column "used" may be less than the correct valueEXT_EP-9752
Compiler shell incorrectly claims to support --analyze=callgraphEXT_EP-9399
2D VLA access in IF condition is mishandledEXT_EP-9365
--opt_level=4, plus library compiled with 6.2.x or older, can cause no-match-for-UMULT errorEXT_EP-8030
Custom boot routine that works with 4.3.x fails with 4.4.xEXT_EP-8032
GCC cast-to-union wrongly rejected in initialization constantEXT_EP-8031
Resource conflict between instruction in SPLOOP and instruction in its epilog causing hardware exceptionEXT_EP-8038
opt470 experienced a segmentation faultEXT_EP-8231
Unsigned array index not truncated properly in array indexing expressionEXT_EP-8233
Float variables allocated to FPU register such as R4H are displayed as "unknown register R4HL" in Variables viewEXT_EP-8230
Remove --symdebug:coff from the compiler manualEXT_EP-8041
MSP430 compiler has an INTERNAL ERROR segmentation fault while parsingEXT_EP-8043
ASG error in cg6xEXT_EP-8244
Value of __cplusplus is wrongEXT_EP-8520
Compiler generates incorrect code for expression that combines int and float typesEXT_EP-8126
ARM compiler incorrectly puts CPSIE and CPSID instructions into an IT blockEXT_EP-8125
Compiler invalidly emits MISRA diagnostic 10.2 The value of an expression of floating type shall not be implicitly convertedEXT_EP-8128
Call to math function (e.g sqrt) using FPUfastRTS leads to redefined symbol "sqrt"EXT_EP-8127
Dwarf debug information incorrectly removed for static data symbol when building with -o3 --gen_func_subsectionsEXT_EP-8133
Assembler incorrectly issues error: Address must be of a non-global defined in the current sectionEXT_EP-8132
Assembler incorrectly issues warning on large constant used with MOVI32 instructionEXT_EP-8135
#pragma FUNCTION_OPTIONS meaningless unless at least -o0 is usedEXT_EP-8134
Compiler incorrectly issues error message when it sees a designated initializer used for a union nested inside a structureEXT_EP-8131
TI ARM compiler fails to build libraryEXT_EP-8130
Compiler generates software pipelined loop that has multiple assignment code, and is not interrupt safeEXT_EP-8137
Performance loss because of register pressure in software pipeline loopEXT_EP-8144
MSP430 ULP Advisor mistakenly says to use type int16_t, when it means uint16_tEXT_EP-8143
Documentation error: #pragma pack should be lower caseEXT_EP-8449
Accepts invalid CLA instruction "MMOV32 MRx, MSTF"EXT_EP-8746
div() and ldiv() return incorrect result when built with -o4 optionEXT_EP-8747
runtime failure; timeoutEXT_EP-8609
_Pragma doesn't support raw string argumentsEXT_EP-8608
C++ header file cuchar is not provided in libc++EXT_EP-8601
libc++ has incorrect implementation of pointer_safetyEXT_EP-8600
owner_less shouldn't inherit from binary_functionEXT_EP-8459
Documentation should state that users must use far keyword when declaring C/C++ data symbols defined by the linkerEXT_EP-8065
Standard library headers may cause errors with the --float_operations_allowed optionEXT_EP-8068
Optimizer Aborts with OUT OF MEMORY ERROREXT_EP-8063
In certain cases at opt_level=2 or higher, compiler gets load and store instructions in the wrong orderEXT_EP-8136
Performance degradation because of incomplete analysis
{"searchers":{"groups":[{"searchers":[{"name":"Project","id":"project","key":"issue.field.project","isShown":true,"lastViewed":1791460751821,"shown":true},{"name":"Summary","id":"summary","key":"issue.field.summary","isShown":true,"shown":true},{"name":"Type","id":"issuetype","key":"issue.field.issuetype","isShown":true,"lastViewed":1791460751822,"shown":true},{"name":"Status","id":"status","key":"issue.field.status","isShown":true,"lastViewed":1791460751831,"shown":true},{"name":"Priority","id":"priority","key":"issue.field.priority","isShown":true,"shown":true},{"name":"Resolution","id":"resolution","key":"issue.field.resolution","isShown":true,"shown":true},{"name":"Creator","id":"creator","key":"issue.field.creator","isShown":true,"shown":true},{"name":"Affects Version","id":"version","key":"issue.field.affectsversions","isShown":false,"shown":false},{"name":"Fix Version","id":"fixfor","key":"issue.field.fixversions","isShown":false,"shown":false},{"name":"Component","id":"component","key":"issue.field.components","isShown":false,"shown":false},{"name":"% Limits","id":"workratio","key":"issue.field.workratio","isShown":true,"shown":true},{"name":"Link types","id":"issue_link_type","key":"issue.field.issuelinks","isShown":true,"shown":true},{"name":"Environment","id":"environment","key":"issue.field.environment","isShown":true,"shown":true},{"name":"Description","id":"description","key":"issue.field.description","isShown":true,"shown":true},{"name":"Comment","id":"comment","key":"issue.field.comment","isShown":true,"shown":true},{"name":"Query","id":"text","key":"text","isShown":true,"shown":true},{"name":"Affected Platform/Device","id":"customfield_10000","key":"com.atlassian.jira.plugin.system.customfieldtypes:textarea","isShown":true,"shown":true},{"name":"Decline Reason","id":"customfield_10001","key":"com.atlassian.jira.plugin.system.customfieldtypes:textarea","isShown":true,"shown":true},{"name":"Development","id":"customfield_10206","key":"com.atlassian.jira.plugins.jira-development-integration-plugin:devsummary","isShown":true,"shown":true},{"name":"Epic Colour","id":"customfield_10204","key":"com.pyxis.greenhopper.jira:gh-epic-color","isShown":false,"shown":false},{"name":"Epic Link","id":"customfield_10201","key":"com.pyxis.greenhopper.jira:gh-epic-link","isShown":true,"shown":true},{"name":"Epic Name","id":"customfield_10203","key":"com.pyxis.greenhopper.jira:gh-epic-label","isShown":true,"shown":true},{"name":"Epic Status","id":"customfield_10202","key":"com.pyxis.greenhopper.jira:gh-epic-status","isShown":false,"shown":false},{"name":"Fix In Release","id":"customfield_10002","key":"com.atlassian.jira.plugin.system.customfieldtypes:textarea","isShown":true,"shown":true},{"name":"Forum URL","id":"customfield_10003","key":"com.atlassian.jira.plugin.system.customfieldtypes:textarea","isShown":true,"shown":true},{"name":"Found In Release","id":"customfield_10004","key":"com.atlassian.jira.plugin.system.customfieldtypes:textarea","isShown":true,"shown":true},{"name":"Internal ID","id":"customfield_10005","key":"com.atlassian.jira.plugin.system.customfieldtypes:textfield","isShown":true,"shown":true},{"name":"OldID","id":"customfield_10102","key":"com.atlassian.jira.plugin.system.customfieldtypes:textfield","isShown":true,"shown":true},{"name":"Original story points","id":"customfield_10211","key":"com.atlassian.jpo:jpo-custom-field-original-story-points","isShown":true,"shown":true},{"name":"Parent Link","id":"customfield_10208","key":"com.atlassian.jpo:jpo-custom-field-parent","isShown":false,"shown":false},{"name":"Product","id":"customfield_10101","key":"com.atlassian.jira.plugin.system.customfieldtypes:textfield","isShown":true,"lastViewed":1791460751834,"shown":true},{"name":"Rank","id":"customfield_10205","key":"com.pyxis.greenhopper.jira:gh-lexo-rank","isShown":true,"shown":true},{"name":"Reason for Unpublish","id":"customfield_10100","key":"com.atlassian.jira.plugin.system.customfieldtypes:textarea","isShown":false,"shown":false},{"name":"Release Notes","id":"customfield_10006","key":"com.atlassian.jira.plugin.system.customfieldtypes:textarea","isShown":true,"shown":true},{"name":"Sprint","id":"customfield_10200","key":"com.pyxis.greenhopper.jira:gh-sprint","isShown":true,"shown":true},{"name":"Team","id":"customfield_10207","key":"com.atlassian.teams:rm-teams-custom-field-team","isShown":true,"shown":true},{"name":"Workaround","id":"customfield_10007","key":"com.atlassian.jira.plugin.system.customfieldtypes:textarea","isShown":true,"shown":true}],"type":"DETAILS","title":"Details"},{"searchers":[{"name":"Created Date","id":"created","key":"issue.field.created","isShown":true,"shown":true},{"name":"Updated Date","id":"updated","key":"issue.field.updated","isShown":true,"shown":true},{"name":"Resolution Date","id":"resolutiondate","key":"issue.field.resolution.date","isShown":true,"shown":true},{"name":"Due Date","id":"duedate","key":"issue.field.duedate","isShown":true,"shown":true},{"name":"Target end","id":"customfield_10210","key":"com.atlassian.jpo:jpo-custom-field-baseline-end","isShown":true,"shown":true},{"name":"Target start","id":"customfield_10209","key":"com.atlassian.jpo:jpo-custom-field-baseline-start","isShown":true,"shown":true}],"type":"DATES","title":"Dates"},{"searchers":[{"name":"Assignee","id":"assignee","key":"issue.field.assignee","isShown":true,"lastViewed":1791460751832,"shown":true},{"name":"Reporter","id":"reporter","key":"issue.field.reporter","isShown":true,"shown":true}],"type":"PEOPLE","title":"People"}]},"values":{"issuetype":{"name":"Type","editHtml":"\n\n\n\n <div class=\"field-group aui-field-issuetype\" >\n <label for=\"searcher-type\">Type</label> <select class=\"select js-default-checkboxmultiselect\"\n id=\"searcher-type\"\n multiple=\"multiple\"\n name=\"type\"\n data-max-inline-results-displayed=\"100\"\n data-placeholder-text=\"Find Issue Types...\">\n <optgroup>\n \n <option class=\" \"\n id=\"type_-2\"\n title=\"All Standard Issue Types\"\n value=\"-2\">All Standard Issue Types</option>\n </optgroup>\n\n <optgroup label=\"Standard Issue Types\">\n \n <option class=\" imagebacked 10308 \"\n data-icon=\"/jira/secure/viewavatar?size=xsmall&avatarId=10600&avatarType=issuetype\"\n data-fallback-icon=\"/jira/images/icons/issuetypes/blank.png\"\n id=\"type_10100\"\n title=\"Bug\"\n value=\"10100\">Bug</option>\n \n <option class=\" imagebacked 10308 \"\n data-icon=\"/jira/secure/viewavatar?size=xsmall&avatarId=10307&avatarType=issuetype\"\n data-fallback-icon=\"/jira/images/icons/issuetypes/blank.png\"\n id=\"type_10101\"\n title=\"Enhancement\"\n value=\"10101\">Enhancement</option>\n \n <option class=\" imagebacked 10202 \"\n data-icon=\"/jira/secure/viewavatar?size=xsmall&avatarId=10320&avatarType=issuetype\"\n data-fallback-icon=\"/jira/images/icons/issuetypes/blank.png\"\n id=\"type_10000\"\n title=\"FAQ\"\n value=\"10000\">FAQ</option>\n </optgroup>\n\n <optgroup label=\"Sub-Task Issue Types\">\n </optgroup>\n </select>\n </div>\n ","validSearcher":true,"isShown":true},"project":{"name":"Project","editHtml":" \n <div class=\"field-group aui-field-project\" >\n <label for=\"searcher-pid\">Project</label> <select class=\"js-project-checkboxmultiselect\"\n data-placeholder-text=\"Find Projects...\"\n id=\"searcher-pid\"\n multiple=\"multiple\"\n name=\"pid\">\n <optgroup label=\"All Projects\" >\n \n <option data-icon=\"/jira/secure/projectavatar?pid=10314&size=small\"\n title=\"Embedded Software & Tools\"\n value=\"10314\">\n Embedded Software & Tools (EXT_EP)\n </option>\n <option data-icon=\"/jira/secure/projectavatar?pid=10600&size=small\"\n title=\"EXT_AUTORADAR_MCAL\"\n value=\"10600\">\n EXT_AUTORADAR_MCAL (EXT_AUTORADAR)\n </option>\n <option data-icon=\"/jira/secure/projectavatar?pid=11101&size=small\"\n title=\"EXT_EDGEAI_ROBOTICS\"\n value=\"11101\">\n EXT_EDGEAI_ROBOTICS (EXEAIR)\n </option>\n <option data-icon=\"/jira/secure/projectavatar?pid=10900&size=small\"\n title=\"EXT_EDGEST\"\n value=\"10900\">\n EXT_EDGEST (EXT_EDGEST)\n </option>\n <option data-icon=\"/jira/secure/projectavatar?pid=10400&size=small\"\n title=\"EXT_LPAA_CS\"\n value=\"10400\">\n EXT_LPAA_CS (EXT_LPAA_CS)\n </option>\n <option data-icon=\"/jira/secure/projectavatar?pid=11300&size=small\"\n title=\"EXT_MSPSWSL\"\n value=\"11300\">\n EXT_MSPSWSL (EXT_MSPSWSL)\n </option>\n <option data-icon=\"/jira/secure/projectavatar?pid=10801&size=small\"\n title=\"EXT_PSDKQA\"\n value=\"10801\">\n EXT_PSDKQA (EXT_PSDKQA)\n </option>\n <option data-icon=\"/jira/secure/projectavatar?pid=11100&size=small\"\n title=\"EXT_SYSFW\"\n value=\"11100\">\n EXT_SYSFW (EXT_SYSFW)\n </option>\n <option data-icon=\"/jira/secure/projectavatar?pid=10800&size=small\"\n title=\"EXT_TSMU8xxA045\"\n value=\"10800\">\n EXT_TSMU8xxA045 (EXT_TSMU)\n </option>\n <option data-icon=\"/jira/secure/projectavatar?pid=10003&size=small\"\n title=\"FAQ\"\n value=\"10003\">\n FAQ (FAQ)\n </option>\n <option data-icon=\"/jira/secure/projectavatar?pid=10700&size=small\"\n title=\"MCU REQ\"\n value=\"10700\">\n MCU REQ (EXT_MCUREQ)\n </option>\n <option data-icon=\"/jira/secure/projectavatar?pid=10500&size=small\"\n title=\"MCU+ SDK\"\n value=\"10500\">\n MCU+ SDK (EXT_MCUSDK)\n </option>\n <option data-icon=\"/jira/secure/projectavatar?pid=11200&size=small\"\n title=\"MSPMCAL\"\n value=\"11200\">\n MSPMCAL (EXT_MSPMCAL)\n </option>\n <option data-icon=\"/jira/secure/projectavatar?pid=11000&size=small\"\n title=\"Sitara MPU & SPMCU SDKs\"\n value=\"11000\">\n Sitara MPU & SPMCU SDKs (EXT_SITMPUSW)\n </option>\n </optgroup>\n </select>\n </div>\n \n\n","validSearcher":true,"isShown":true},"assignee":{"name":"Assignee","editHtml":"\n \n <div class=\"field-group aui-field-userlist\" >\n <label for=\"searcher-assigneeSelect\">Assignee</label> <fieldset rel=\"assignee\" class=\"hidden user-group-searcher-params\">\n </fieldset>\n <select class=\"js-usergroup-checkboxmultiselect\" multiple=\"multiple\" id=\"assignee\" name=\"assignee\" data-placeholder-text=\"Enter username or group\">\n <optgroup>\n <option class=\"headerOption\" data-icon=\"https://sir.ext.ti.com/jira/secure/useravatar?size=xsmall&avatarId=10123\" value=\"empty\" title=\"Unassigned\">Unassigned</option>\n </optgroup>\n <optgroup>\n </optgroup>\n </select>\n <input type=\"hidden\" name=\"check_prev_assignee\" value=\"true\">\n </div>\n \n","validSearcher":true,"isShown":true},"customfield_10101":{"name":"Product","viewHtml":"\n\n\n <div class=\"searcherValue\">\n \n <label class=\"fieldLabel\" for=\"fieldcustomfield_10101\">Product:</label><span id=\"fieldcustomfield_10101\" class=\"fieldValue \">\n \nCode Generation Tools\n</span></div>\n","editHtml":"\n <div class=\"field-group aui-field-text\" >\n <label for=\"searcher-customfield_10101\">Product</label> <input class=\"text\" id=\"searcher-customfield_10101\" name=\"customfield_10101\" type=\"text\" value=\"Code Generation Tools\" />\n </div>\n ","jql":"Product ~ \"Code Generation Tools\"","validSearcher":true,"isShown":true},"status":{"name":"Status","editHtml":"\n <div class=\"field-group aui-field-constants\" >\n <label for=\"searcher-status\">Status</label> <select class=\"select js-default-checkboxmultiselectstatuslozenge\"\n data-placeholder-text=\"Find Statuses...\"\n id=\"searcher-status\"\n multiple=\"multiple\"\n name=\"status\"\n data-max-inline-results-displayed=\"100\"\n data-footer-text=\"-88 more options. Continue typing to refine further.\" data-status-lozenge=\"true\">\n <optgroup >\n <option class=\"imagebacked\" data-icon=\"/jira/images/icons/statuses/inprogress.png\" value=\"3\" title=\"In Progress\" data-simple-status=\"{"id":"3","name":"In Progress","description":"This issue is being actively worked on at the moment by the assignee.","iconUrl":"/jira/images/icons/statuses/inprogress.png","statusCategory":{"id":4,"key":"indeterminate","colorName":"inprogress"}}\">In Progress</option>\n <option class=\"imagebacked\" data-icon=\"/jira/images/icons/status_generic.gif\" value=\"10000\" title=\"To Do\" data-simple-status=\"{"id":"10000","name":"To Do","description":"","iconUrl":"/jira/images/icons/status_generic.gif","statusCategory":{"id":2,"key":"new","colorName":"default"}}\">To Do</option>\n <option class=\"imagebacked\" data-icon=\"/jira/images/icons/status_generic.gif\" value=\"10001\" title=\"Published\" data-simple-status=\"{"id":"10001","name":"Published","description":"","iconUrl":"/jira/images/icons/status_generic.gif","statusCategory":{"id":3,"key":"done","colorName":"success"}}\">Published</option>\n <option class=\"imagebacked\" data-icon=\"/jira/images/icons/status_generic.gif\" value=\"10100\" title=\"Accepted\" data-simple-status=\"{"id":"10100","name":"Accepted","description":"","iconUrl":"/jira/images/icons/status_generic.gif","statusCategory":{"id":4,"key":"indeterminate","colorName":"inprogress"}}\">Accepted</option>\n <option class=\"imagebacked\" data-icon=\"/jira/images/icons/status_generic.gif\" value=\"10101\" title=\"Declined\" data-simple-status=\"{"id":"10101","name":"Declined","description":"","iconUrl":"/jira/images/icons/status_generic.gif","statusCategory":{"id":3,"key":"done","colorName":"success"}}\">Declined</option>\n <option class=\"imagebacked\" data-icon=\"/jira/images/icons/status_generic.gif\" value=\"10102\" title=\"Fixed\" data-simple-status=\"{"id":"10102","name":"Fixed","description":"","iconUrl":"/jira/images/icons/status_generic.gif","statusCategory":{"id":3,"key":"done","colorName":"success"}}\">Fixed</option>\n <option class=\"imagebacked\" data-icon=\"/jira/images/icons/status_generic.gif\" value=\"10103\" title=\"In Development\" data-simple-status=\"{"id":"10103","name":"In Development","description":"","iconUrl":"/jira/images/icons/status_generic.gif","statusCategory":{"id":4,"key":"indeterminate","colorName":"inprogress"}}\">In Development</option>\n <option class=\"imagebacked\" data-icon=\"/jira/images/icons/status_generic.gif\" value=\"10104\" title=\"New\" data-simple-status=\"{"id":"10104","name":"New","description":"","iconUrl":"/jira/images/icons/status_generic.gif","statusCategory":{"id":2,"key":"new","colorName":"default"}}\">New</option>\n <option class=\"imagebacked\" data-icon=\"/jira/images/icons/status_generic.gif\" value=\"10105\" title=\"On Hold\" data-simple-status=\"{"id":"10105","name":"On Hold","description":"","iconUrl":"/jira/images/icons/status_generic.gif","statusCategory":{"id":4,"key":"indeterminate","colorName":"inprogress"}}\">On Hold</option>\n <option class=\"imagebacked\" data-icon=\"/jira/images/icons/status_generic.gif\" value=\"10106\" title=\"Implemented\" data-simple-status=\"{"id":"10106","name":"Implemented","description":"","iconUrl":"/jira/images/icons/status_generic.gif","statusCategory":{"id":3,"key":"done","colorName":"success"}}\">Implemented</option>\n <option class=\"imagebacked\" data-icon=\"/jira/images/icons/status_generic.gif\" value=\"10107\" title=\"Planned\" data-simple-status=\"{"id":"10107","name":"Planned","description":"","iconUrl":"/jira/images/icons/status_generic.gif","statusCategory":{"id":4,"key":"indeterminate","colorName":"inprogress"}}\">Planned</option>\n <option class=\"imagebacked\" data-icon=\"/jira/images/icons/statuses/generic.png\" value=\"10200\" title=\"Unpublished\" data-simple-status=\"{"id":"10200","name":"Unpublished","description":"","iconUrl":"/jira/images/icons/statuses/generic.png","statusCategory":{"id":3,"key":"done","colorName":"success"}}\">Unpublished</option>\n </optgroup>\n</select>\n </div>\n \n","validSearcher":true,"isShown":true}},"queryFitsFilterForm":true}
[{"id":-1,"name":"My open issues","jql":"assignee = currentUser() AND resolution = Unresolved order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":true},{"id":-2,"name":"Reported by me","jql":"reporter = currentUser() order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":true},{"id":-4,"name":"All issues","jql":"order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-5,"name":"Open issues","jql":"resolution = Unresolved order by priority DESC,updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-9,"name":"Done issues","jql":"statusCategory = Done order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-3,"name":"Viewed recently","jql":"issuekey in issueHistory() order by lastViewed DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-6,"name":"Created recently","jql":"created >= -1w order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-7,"name":"Resolved recently","jql":"resolutiondate >= -1w order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-8,"name":"Updated recently","jql":"updated >= -1w order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false}]
0.3
0