Float variables allocated to FPU register such as R4H are displayed as "unknown register R4HL" in Variables view

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-1927
    • Hide
      C2000_16.6.0.STS
       C2000_15.12.0.LTS
       C2000_6.4.0B1
      Show
      C2000_16.6.0.STS  C2000_15.12.0.LTS  C2000_6.4.0B1
    • Hide
      C2000_6.4.12
       C2000_15.12.5.LTS
       C2000_16.9.2.LTS
      Show
      C2000_6.4.12  C2000_15.12.5.LTS  C2000_16.9.2.LTS
    • Lowering the level of optimization in the project such that the variable is not allocated to a register will allow its value to be displayed correctly in the Variables view.
    • Fixed an issue where FPU32 registers were sometimes incorrectly named and not available during debug.

      Float variables allocated to FPU register such as R4H are displayed as "unknown register R4HL" in Variables view

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-736 - Float variables allocated to FPU re...
                SYNCHRONIZED
                • Last Sync Date: