Compiler fails with INTERNAL ERROR: ac2000 experienced a segmentation fault

XMLWordPrintable

    • Type: Bug
    • Resolution: Duplicate
    • Priority: Medium

      Use the attached files.

      % cl2000 -@options.txt try1.c
      "try1.c", line 22899 (col. 54): advice #2615-D: (Performance) Use --fp_mode=relaxed to enable TMU hardware support for FP division.
      
      INTERNAL ERROR: ac2000 experienced a segmentation fault
                        while processing function (unknown or file scope) file (unknown) line 0
      
      This is caused by a defect in the TI C/C++ Parser.
      TI Customer Support may be able to suggest a workaround to avoid this.
      
      Upgrading to the newest version of the compiler may fix this problem.
      
      Contact TI in the E2E support forums at http://e2e.ti.com under
      "Development Tools", "TI C/C++ Compiler".  See the link titled
      "Submitting an issue".
      
      We need to see this ENTIRE error message and a complete, reproducible
      test case including ALL of the command-line options.
      Include the .pp file created by option --preproc_with_comment
      
      
      >> Compilation failure
      

      Note the problem does not occur when using version 19.6.0.STS.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2250 - Compiler fails with INTERNAL ERROR:...
                SYNCHRONIZED
                • Last Sync Date: