Export - CSV (All fields)
Export - CSV (Current fields)
EXT_EP-11464
Newly added images to the dataset are added with string IDs causing Training fails because some images have string instead of integer IDs causing training errorsEXT_EP-11227
Editing id in Annotations dialog box duplicates the number of rows in the tableEXT_EP-11617
User sees 'Uploading project...' modal if they refresh page in middle of uploadEXT_EP-11800
Support SDK 9.2.0 in Model ComposerEXT_EP-11230
No error message for unsupported cameraEXT_EP-12160
Can't Delete Images Unless They Are SelectedEXT_EP-12162
Graphs on capture, live preview page are white in dark mode pageEXT_EP-11769
[Model Analyzer] Jupyter notebooks for model evaluations are getting disconnected frequentlyEXT_EP-12254
Provide usable UI if MC Extension does not require compilation propertiesEXT_EDGEST-2
Object detection : Annotation label pop up not visibleEXT_EP-12357
User-defined manual train/val/test set split support for vision Model MakerEXT_EP-12365
Surface Classification training engine should support train/val/test assignmentsEXT_EP-12364
robust data collection with 250kHz sampling rate at 9M baudEXT_EP-12403
Ensure that the localized versions of dialogs have the same text as the english textEXT_EP-12601
Define a project ordering in project list that makes sense to a userEXT_EP-12656
Negative "unannotated" images after annotating 20k images block trainingEXT_EP-12713
Zooming into graph while doing vibration collection stops drawing the signalEXT_EP-12763
Compile Tab's Text Scaling IssueEXT_EP-12766
mmwave training reports in batches of 30 epochs. Graph is usually not complete.EXT_EP-12924
What's New Dialog and content contribution and update schemeEXT_EP-12923
Training process to provide feedback on which data files caused false alarmsEXT_EP-13269
Cannot cancel and restart training or compile tasks in new UI training listEXT_EP-13281
What's new Panel requires users to go through "I am a human being" process to see the Content.EXT_EP-13282
When train session completes in the cloud, I cannot start a new sessionEXT_EP-13274
Annotation: Unable to assign split after assigning a class labelEXT_EP-13323
"Rows per page" and the sorted column settings gets reset when a user opens a project and then navigates back to the home pageEXT_EP-13324
Issues with training runs with F29 in v1.6.0EXT_EP-13276
The new UI is missing the ability to create a new training run or compile run from an existing one.EXT_EP-13322
Renaming the session does not work for projects with train and compile sessions created with 1.5 codeEXT_EP-13329
Prematurely stopping the capture with the "Stop Capture" button does not write existing data to a fileEXT_EP-13332
There is no way to export a data setEXT_EP-13333
On cloud, device selection in wizard is not retained on FirefoxEXT_EP-13335
MOSFET Temperature Prediction example project fails to train on both desktop and cloudEXT_EP-13336
Grid Fault Detection example project fails to train on both desktop and cloudEXT_EP-13337
Old UI does not show progress for TinyML examplesEXT_EP-13339
Need a way / button to go back to landing page from timeseries page. Need a way/button to go back to landing page from old UI page.EXT_EP-13350
Compiled model artifacts fail to export to a CCS project if the project is missing an expected directoryEXT_EP-13351
New UI (cloud) - Missing function to export compiled artifacts to cloud CCSEXT_EP-13352
Start capture button on the properties button gets disabled after flipping tabsEXT_EP-13353
Capture/preview dropdown options list box is off from text box when resizing a panel
{"errorMessages":["jqlTooComplex"],"errors":{}}
[{"id":-1,"name":"My open issues","jql":"assignee = currentUser() AND resolution = Unresolved order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":true},{"id":-2,"name":"Reported by me","jql":"reporter = currentUser() order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":true},{"id":-4,"name":"All issues","jql":"order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-5,"name":"Open issues","jql":"resolution = Unresolved order by priority DESC,updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-9,"name":"Done issues","jql":"statusCategory = Done order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-3,"name":"Viewed recently","jql":"issuekey in issueHistory() order by lastViewed DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-6,"name":"Created recently","jql":"created >= -1w order by created DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-7,"name":"Resolved recently","jql":"resolutiondate >= -1w order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false},{"id":-8,"name":"Updated recently","jql":"updated >= -1w order by updated DESC","isSystem":true,"sharePermissions":[],"requiresLogin":false}]
0.3
0