mmwave training reports in batches of 30 epochs. Graph is usually not complete.

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium
    • Edge AI Studio
    • EDGEST-1405
    • MC_1.4.0
    • None

      The mmwave back end reports epoch results every 30 epochs.   For a training run of 300 epochs the graph is only shown up to 271  see below.    If epochs are changed to 29 only one point will be shown on the graph (see second image).   Ideally the epoch training result reporting would be more frequent so that the graphs are more complete. 

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-5794 - mmwave training reports in batches ...
                SYNCHRONIZED
                • Last Sync Date: