Provide usable UI if MC Extension does not require compilation properties

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium
    • Edge AI Studio
    • EDGEST-1323
    • MC_1.3.1
    • MC_1.4.0
    • None

      Surface Classification the user does not need to specify any compiler options. The MC UI need to be reasonable in that case. 
      One possibility is if the extension provides 0 or 1 compile properties options - to disable the dropdown, since the user doesn't really have an option. 

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-5206 - Provide usable UI if MC Extension d...
                SYNCHRONIZED
                • Last Sync Date: