TIOVX delay parameters with pipelining result in serialization of nodes

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Low
    • OpenVX Framework
    • TIOVX-823
    • TIOVX_01.07.00
    • TIOVX_10.02.00
    • Hide
      j721e-evm
      j721s2-evm
      j784s4-evm
      Show
      j721e-evm j721s2-evm j784s4-evm
    • Internal implementation of delay parameters within a node can be used to avoid this issue. Please refer to the DOF node as an example of how this can be done
    • This is a known issue and not intended to be fixed

      TIOVX delay parameters with pipelining result in serialization nodes even though the data given to node is functionally correct.  For example, the VISS/AEWB node configuration results in the VISS node being executed then AEWB executed in serial rather than in parallel.

      Workaround for delay parameters is to either use graph parameters instead of delay or to utilize a remote server call to pass delay parameter from one node to another.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-2442 - TIOVX delay parameters with pipelin...
                ERROR
                • Last Sync Date: