Compiler may crash if two thread-local accesses in one function are separated by a function call

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-6419
    • Hide
      C6000_8.3.2
       C6000_8.2.6
      Show
      C6000_8.3.2  C6000_8.2.6
    • Hide
      C6000_8.3.5
       C6000_8.2.8
      Show
      C6000_8.3.5  C6000_8.2.8
    • The compiler may crash when given a function with more than one access to any thread-local variable. This bug is not likely to ...

      Compiler may crash if two thread-local accesses in one function are separated by a function call

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-1906 - Compiler may crash if two thread-lo...
                ERROR
                • Last Sync Date: