Warning when using pragma RETAIN with attribute((noinit))

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-4600
    • Hide
      C6000_8.2.0
       ARP32_1.0.9
       C2000_16.9.0.LTS
      Show
      C6000_8.2.0  ARP32_1.0.9  C2000_16.9.0.LTS
    • Hide
      ARP32_1.1.0*
       ARM_18.9.0.STS
       C2000_18.9.0.STS
      Show
      ARP32_1.1.0*  ARM_18.9.0.STS  C2000_18.9.0.STS
    • Hide
      When using pragma RETAIN with attribute((noinit)) on the same symbol for an EABI target, a .clink directive is erroneously emitted in the assembly file, leading to a warning that the .CLINK directive is being ignored because the symbol already has .RETAIN specified.
      Show
      When using pragma RETAIN with attribute((noinit)) on the same symbol for an EABI target, a .clink directive is erroneously emitted in the assembly file, leading to a warning that the .CLINK directive is being ignored because the symbol already has .RETAIN specified.

      Warning when using pragma RETAIN with attribute((noinit))

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-1494 - Warning when using pragma RETAIN wi...
                ERROR
                • Last Sync Date: