Should reject certain unitless instructions in parallel with certain other instructions

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Low
    • Code Generation Tools
    • CODEGEN-747
    • SDSCM00048041
    • Hide
      C6000_8.2.0
      C6000_8.3.0
      C6000_8.1.0B1
      C6000_7.4.0B1
      Show
      C6000_8.2.0 C6000_8.3.0 C6000_8.1.0B1 C6000_7.4.0B1

      C66x DSP CPU and Instruction Set Reference Guide (SPRUGH7 Nov 2010) section 3.8.12 (and subsections) has a long list of instructions that may not go in parallel, such as "DINT||NOP 5". The assembler does not detect some of these erroneous sequences and so therefore will not emit an error if such a sequence occurs in assembly. The C/C++ compiler does not produce these sequences when compiling C or C+, so the user of the compiler can safely assume these sequences won't occur if only compiling C or C+ code.

      For example, the assembler does not detect the following erroneous sequences:

       ; asm does not detect erroneous sequence
         IDLE
      ||  NOP 2
      
       ; asm does not detect erroneous sequence
          NOP 3
      ||  SWE
      
       ; asm does not detect erroneous sequence
          RINT
      ||  MVC.S2 B0, TSR
      

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-313 - Should reject certain unitless inst...
                ERROR
                • Last Sync Date: