Compiler does not support characters in the ISO 8859 extended character set

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium

      The documentation on support for characters states:

      Characters in the ISO 8859 extended character set are also supported.

      But for this source code ...

      /* The last character in this string is tilde-N */
      char test_string[] = "tilde-N: ñ";
      

      The compiler issues this diagnostic ...

      % tiarmclang -c file.c
      file.c:2:32: warning: illegal character encoding in string literal [-Winvalid-source-encoding]
      char test_string[] = "tilde-N: <F1>";
                                     ^~~~
      1 warning generated.
      

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4679 - Compiler does not support character...
                ERROR
                • Last Sync Date: