Include FreeRTOS kernel source files in Core SDK

XMLWordPrintable

    • Type: Enhancement
    • Resolution: Implemented
    • Priority: Medium
    • TI Device Drivers
    • TIDRIVERS-6134
    • TIDRIVERS_7_40_00
    • Hide
      CC32xx
      CC13x1
      CC26x1
      CC13x2
      CC26x2
      CC13x2x7
      CC26x2x7
      CC13x4
      CC26x3
      CC26x4
      CC23x0
      CC23x1
      CC27x4
      CC27x5
      CC35x0
      CC35x1
      Show
      CC32xx CC13x1 CC26x1 CC13x2 CC26x2 CC13x2x7 CC26x2x7 CC13x4 CC26x3 CC26x4 CC23x0 CC23x1 CC27x4 CC27x5 CC35x0 CC35x1

      The end user is currently expected to separately download FreeRTOS and specify its location in their IDE.

      This feature includes shipping the FreeRTOS source files in the source/third_party/freertos folder. SysConfig understands automatically how to find and import them.

      This means that the old FREERTOS_INSTALL_DIR define is no longer required and will be ignored if set. A different version of FreeRTOS can still be used by setting a relative path to its source files via SysConfig.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4229 - Include FreeRTOS kernel source file...
                SYNCHRONIZED
                • Last Sync Date: