BUILD_MPU flag removed from codebase

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • MCAL
    • MCAL-8198
    • MCUSW_J7_01.03.04
    • MCUSW_J7_09.00.00
    • j721e-evm
    • Hide
      Removed BUILD_MPU flags from code and build system.
      done the system validation.
      Show
      Removed BUILD_MPU flags from code and build system. done the system validation.

      The MPU build option has been deprecated as building for the A72 baremetal is no longer supported. However, the definitions are still present in the project, for example in the MemMap header files. All required code for MPU builds should be removed.

       

      For example, any BUILD_MPU flags should be removed from code and build system. Unnecessary preprocessor definitions such as "CAN_FUNC_TEXT_SECTION" are no longer needed and should be removed from code as well.

       

      Customer (Elektrobit) had issues with custom code in the MemMap headers that would otherwise not be generated by an AUTOSAR vendor, this fix would also make the headers compatible for their generation.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3939 - BUILD_MPU flag removed from codebase
                ERROR
                • Last Sync Date: