Frame Freeze in QNX when LDC node, Mosaic node and a Display node added to SRV demo

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium
    • OpenVX Framework
    • TIOVX-1238
    • TIOVX_08.02.00
    • TIOVX_09.02.00
    • Hide
      j721e-evm
      j721s2-evm
      j784s4-evm
      Show
      j721e-evm j721s2-evm j784s4-evm
    • This is a known issue, but there is a patch available for this. Integrating this patch though can cause issues related to other use cases, so will mark it only in release notes and provide patch if needed

      When we run the SRV demo i.e. "./run_app_srv.sh" in QNX + RTOS SDK after applying the attached patch "Working_SRV_V1.patch" in vision_apps, we observe a frame freeze.

      The same runs fine in the Linux + RTOS SDK.

      Update 9/15: Confirmed on Lucas's setup that this is successful on 8.2 Linux + RTOS.  However, it is failing on 8.4 Linux + RTOS

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-3629 - Frame Freeze in QNX when LDC node, ...
                ERROR
                • Last Sync Date: