[EXT_EP-10990] Frame Freeze in QNX when LDC node, Mosaic node and a Display node added to SRV demo Created: 16/Dec/22  Updated: 20/Aug/24

Status: Declined
Project: Embedded Software & Tools
Component/s: None
Affects Version/s: None
Fix Version/s: None

Type: Bug Priority: Medium
Reporter: TI User Assignee: TI User
Resolution: Unresolved Votes: 0
Remaining Estimate: Not Specified
Time Spent: Not Specified
Original Estimate: Not Specified

Product: OpenVX Framework
Internal ID: TIOVX-1238
Found In Release: TIOVX_08.02.00
Fix In Release: TIOVX_09.02.00
Affected Platform/Device: j721e-evm
j721s2-evm
j784s4-evm
Decline Reason: This is a known issue, but there is a patch available for this. Integrating this patch though can cause issues related to other use cases, so will mark it only in release notes and provide patch if needed

 Description   

When we run the SRV demo i.e. "./run_app_srv.sh" in QNX + RTOS SDK after applying the attached patch "Working_SRV_V1.patch" in vision_apps, we observe a frame freeze.

The same runs fine in the Linux + RTOS SDK.

Update 9/15: Confirmed on Lucas's setup that this is successful on 8.2 Linux + RTOS.  However, it is failing on 8.4 Linux + RTOS


Generated at Wed Apr 09 03:41:07 CDT 2025 using Jira 9.12.17#9120017-sha1:aba4002bcd633f188b6a4bb5dd8a0e1f20b79ee4.