Intermittent, but repeatable failures TIOVX in conformance tests

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • OpenVX Framework
    • TIOVX-1241
    • TIOVX_08.02.00
    • TIOVX_09.01.00
    • j721e-evm

      If a subset of the TI OpenVX Conformance tests is run in a continuous loop there are a few issues, possibly associated with a memory leak.

      Here are the results:
      It was running constantly all the time, so there was no hangs. When interrupted the execution of test suit, it was 1034 iterations done of selected test suit. However it was only 33 iterations completed with all tests passed with success. Since iteration nr. 34 some tests start failing(170 tests passed and 2 tests failed for iteration 34 or 39 tests passed and 133 tests failed since iteration 45). This scenario keeps continue till the last iteration nr. 1034 and the number of failing tests is increasing.

      First fail:
      tiovx-first-fail.jpg

      Subsequent fails:
      tiovx-subsequent-fail1.jpg
      tiovx-subsequent-fail2.jpg

      Please unzip tiovx_conf_log00.zip for the full log.

       

      Update 9/19: when this was run on 8.4, this failed at iteration #52

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3628 - Intermittent, but repeatable failur...
                ERROR
                • Last Sync Date: