[EXT_EP-10989] Intermittent, but repeatable failures TIOVX in conformance tests Created: 16/Dec/22  Updated: 07/Dec/23  Resolved: 07/Dec/23
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
Product: OpenVX Framework
Internal ID: TIOVX-1241
Found In Release: TIOVX_08.02.00
Fix In Release: TIOVX_09.01.00
Affected Platform/Device: j721e-evm

 Description   

If a subset of the TI OpenVX Conformance tests is run in a continuous loop there are a few issues, possibly associated with a memory leak.

Here are the results:
It was running constantly all the time, so there was no hangs. When interrupted the execution of test suit, it was 1034 iterations done of selected test suit. However it was only 33 iterations completed with all tests passed with success. Since iteration nr. 34 some tests start failing(170 tests passed and 2 tests failed for iteration 34 or 39 tests passed and 133 tests failed since iteration 45). This scenario keeps continue till the last iteration nr. 1034 and the number of failing tests is increasing.

First fail:
tiovx-first-fail.jpg

Subsequent fails:
tiovx-subsequent-fail1.jpg
tiovx-subsequent-fail2.jpg

Please unzip tiovx_conf_log00.zip for the full log.

 

Update 9/19: when this was run on 8.4, this failed at iteration #52


Generated at Sat Dec 13 11:39:10 CST 2025 using Jira 10.3.7#10030007-sha1:a563685562f94d165eb4e158cfb2a142338d8c54.