Under certain conditions the CC2652R1 failed to synchronize to periodic advertising

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium
    • SimpleLink CC13x2-26x2 SDK BLE5 Stack
    • BLE_AGAMA-3774
    • BLE Stack BLE5-2.2.4 RC9
    • CC2652R1

      Under certain conditions the CC2652R1 failed to synchronize to periodic advertising. The behavior is typically observed when the CTE count is low.

      During testing, the Central device is sending Advertising PDU and tries to synchronize to the Periodic Advertising PDU sent by the Peripheral device.
      In some cases the synchronization is failed. If the synchronization is established - it will lost soon after.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-3428 - Under certain conditions the CC2652...
                SYNCHRONIZED
                • Last Sync Date: