ECDSACC26X2 Sysconfig does not configure ECDSACC26X2_HWAttrs.trngIntPriority

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • TI Device Drivers
    • TIDRIVERS-4695
    • TIDRIVERS_5_20_00
    • TIDRIVERS_5_30_00
    • Hide
      CC13x2
      CC26x2
      Show
      CC13x2 CC26x2
    • SysConfig does not configure ECDSACC26X2_HWAttrs.trngIntPriority. This means that it is set to 0 by default. That results in the ECDSA driver using a zero-latency interrupt while generating its PMSN during signing.

      SysConfig does not configure ECDSACC26X2_HWAttrs.trngIntPriority. This means that it is set to 0 by default. That results in the ECDSA driver using a zero-latency interrupt while generating its PMSN during signing.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2494 - ECDSACC26X2 Sysconfig does not conf...
                SYNCHRONIZED
                • Last Sync Date: