TDEH EXIDX binary search helper reads past the end of EXIDX

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Low
    • Code Generation Tools
    • CODEGEN-7948
    • Hide
      C7000_1.4.0.LTS
      C6000_8.2.0
      C6000_8.3.0
      MSP430_20.2.0.LTS
      ARM_18.12.0.LTS
      MSP430_18.12.0.LTS
      ARM_20.2.0.LTS
      C2000_18.12.0.LTS
      C2000_20.2.0.LTS
      Show
      C7000_1.4.0.LTS C6000_8.2.0 C6000_8.3.0 MSP430_20.2.0.LTS ARM_18.12.0.LTS MSP430_18.12.0.LTS ARM_20.2.0.LTS C2000_18.12.0.LTS C2000_20.2.0.LTS
    • Hide
      C7000_1.4.1.LTS*
      MSP430_18.12.7.LTS*
      ARM_18.12.7.LTS*
      C6000_8.2.10*
      C6000_8.3.8*
      C2000_20.2.3.LTS*
      C2000_18.12.7.LTS*
      ARM_20.2.3.LTS*
      MSP430_20.2.3.LTS*
      Show
      C7000_1.4.1.LTS* MSP430_18.12.7.LTS* ARM_18.12.7.LTS* C6000_8.2.10* C6000_8.3.8* C2000_20.2.3.LTS* C2000_18.12.7.LTS* ARM_20.2.3.LTS* MSP430_20.2.3.LTS*
    • default
    • Edit the RTS file tdeh_unwinder.cpp. In the function __TI_ut_entry_cmp(), remove the second statement that sets next_func_abs. Add this file to your project and recompile.
    • Hide
      The Table-Driven C++ Exception Handling (TDEH) code in the Run-Time Support library (RTS) had a bug where it could read past the end of the EXIDX section when handling a C++ exception. This could cause a bogus, unpredictable result when handling an exception, and it could result in a read outside of configured memory. This bug can only happen in C++, and only when an exception is thrown by the program.
      Show
      The Table-Driven C++ Exception Handling (TDEH) code in the Run-Time Support library (RTS) had a bug where it could read past the end of the EXIDX section when handling a C++ exception. This could cause a bogus, unpredictable result when handling an exception, and it could result in a read outside of configured memory. This bug can only happen in C++, and only when an exception is thrown by the program.

      The Table-Driven C++ Exception Handling (TDEH) code in the Run-Time Support library (RTS) had a bug where it could read past the end of the EXIDX section when handling a C++ exception. This could cause a bogus, unpredictable result when handling an exception, and it could result in a read outside of configured memory. This bug can only happen in C++, and only when an exception is thrown by the program.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2454 - TDEH EXIDX binary search helper rea...
                SYNCHRONIZED
                • Last Sync Date: