Bmp utils do not work for loading RGBX images

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Low
    • OpenVX Framework
    • TIOVX-569
    • TIOVX_01.04.00
    • Hide
      TIOVX_12.02.00
      TDA54.12.01.01.00
      Show
      TIOVX_12.02.00 TDA54.12.01.01.00
    • Hide
      j721e-evm
      j721s2-evm
      j784s4-evm
      j722s-evm
      j742s2-evm
      tda54-evm
      Show
      j721e-evm j721s2-evm j784s4-evm j722s-evm j742s2-evm tda54-evm
    • None

      The utils function for loading a file from bmp does not work properly if the image is RGBX.  The utils assumes that if it is not raw it will be RGB and therefore there is a mismatch if trying to load it to an RGBX formatted vx_image.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-2444 - Bmp utils do not work for loading R...
                SYNCHRONIZED
                • Last Sync Date: