[RTLS] Sometimes there are no Angle reports for all connections when configured to 4-1-1 [aoa_sample_rate-aoa_slot_durations-aoa_sample_size], when working with CCS

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium
    • SimpleLink CC13x2-26x2 SDK BLE5 Stack
    • BLE_AGAMA-1974
    • Hide
      BLE Stack BLE5-2.1.2 RC9
      BLE Stack BLE5-2.1.2
      Show
      BLE Stack BLE5-2.1.2 RC9 BLE Stack BLE5-2.1.2
    • BLE Stack BLE5-2.1.x
    • CC26X2R1

      Reproduced for SDK version 4.10.00.70. Sometimes master is stuck after the test finished: master disconnect timeout. In 3 from 5 times the master stuck reproduced for configuration 3-1-1 also.

      No Angle reports on all eight links for the configuration [4-1-1] [aoa_sample_rate-aoa_slot_durations-aoa_sample_size].

      Note: the same issue occurred for configuration 4-2-2, but was successful for 2-2-2

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-2410 - [RTLS] Sometimes there are no Angle...
                ERROR
                • Last Sync Date: