Multi-role incorrectly sets gapRole_AdvEnabled when enabling non-connectable advertisements.

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium
    • SimpleLink CC2640R2 SDK BLE Stack
    • BLESTACK-2706
    • BLE Stack 3.1.0
    • BLE Stack 3.2.x
    • CC26xxR2

      Multi Role incorrectly setting gapRole_AdvEnabled when enabling non-connectable adv

       

      Git/Installer Release Version:
      simplelink_cc2640r2_sdk_1_40_00_45

      Application:
      multi_role

      Problem Reproducibility:
      100%

      Problem Description:
      On multi.c anytime a GAP_MAKE_DISCOVERABLE_DONE_EVENT is received the gapRole_AdvEnabled flag is set to true even if the advertising is non-connectable. This then prevents us from disabling non-connectable advertising as this checks that connectable advertising must be disabled.

      Looks like this flag may not need to be set at that point as it is set correctly before calling gapRole_setEvent(START_ADVERTISING_EVT) for both connectable and non-connectable advertising.

      Steps to re-create problem:
      Modify multi-role example to use non-connectable advertising (switch GAPROLE_ADVERT_ENABLED -> GAPROLE_ADV_NONCONN_ENABLED) On terminal menu select advertising to attempt to disable advertising. This leads to a bleIncorrectMode return type from GAPRole_SetParameter() and device continues to advertise.

      Link to E2E post where this was found:
      https://e2e.ti.com/support/wireless_connectivity/bluetooth_low_energy/f/538/t/628711

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-2403 - Multi-role incorrectly sets gapRole...
                SYNCHRONIZED
                • Last Sync Date: